cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, is there any way to "enforce" a CubeIDE version in code, e.g. a static_assert()? Regards, Goran

GoEk
Associate III
11 REPLIES 11
GoEk
Associate III

Thanks for the info. Coincidentally, today when I updated to 1.11.0 via the built-in update tool the source files didn't show anymore (editor was "invalid" or something) and there were no build setups with similar error. This installation had been updated from 1.8 up to 1.10 using the built-in tool. I uninstalled and reinstalled a fresh 1.11.0 in the recommended directory and then it works just fine.

Small update on this topic:

Decision has at least been taken to move this info from source- to header-files.

The deployment time depends on the overall release plans for each CubeFW package.

Internal ticket reference: 140908.