cancel
Showing results for 
Search instead for 
Did you mean: 

hi i have stm32f207igh6 and i want to use its ethernet interface , i have the DP83849IFVS , i want to use it with the stm32f207igh6 , when i try to configure the ETH in STM32cubeIDE i can see just two phy , the DP83848 and the LAN8742A , and user phy

Oassa.1
Associate

so how can i configure the DP83849IFVS to work with the stm32f207igh6 using stm32cubeide

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

hello @Oassa.1​ ,

When using the STM32cubeMX, you need to select the PHY -> user PHY in the External PHY Configuration panel.

I hope this helps.

BeST Regards,

Walid