cancel
Showing results for 
Search instead for 
Did you mean: 

FAIL.txt file appears on the disk.

akoluacik
Senior

Once I connect my board(f746-disco), there is a disk in which FAIL.txt appears which contains "The interface firmware FAILED to reset/halt the target MCU". I have been getting this error since yesterday. I found a question asked this community, it was recommended to update STLink. However I did this, the problem is not solved. Moreover, I removed and re-installed CubeIDE, but the problem still continues. When I try to upload a code via Cube IDE, I got

"Error in final launch sequence:

Failed to start GDB server

Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (4) No device found on target."

What can I do? Please help me it is very very urgent, it is vital for me.

Thanks for your help.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
MFran.4
Senior

Is the board powered correctly? (test with multimeter)

Did it stop working or it just never worked?

What does stop working mean? The power led is lighting, but I cannot upload code to board.

Which part/component should I measure on the board?​

And thank you for your answer.​

What changed/happened when it stopped working.

​

C​heck jumpers related to powering board and STM32 chip.

Check ​connectivity of SWD/JTAG pins, see jumpers or solder bridges.

Current measuring jumpers?

Option bytes or Read Out Protection, RDP2 ??​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

To check all these,​ I need to look at schematic, dont I?

I ​have no idea what happened to my board and it stopped working. I just wanted to use built-in microphone, I configured everything, then plug the board to my pc, but I see the text file on the disk :(.

akoluacik
Senior

Update:

I researched more on Google, and saw some suggestion to use ST-Link Utility. At first, I connect NRST pin to 3.3V, and then used erase chip on st-utility, after that I uploaded a code(.hex file) compiled on MBED studio. The code works when I connect NRST to 3.3v, but now ST-Utility cannot see my device.