cancel
Showing results for 
Search instead for 
Did you mean: 

Error in final launch sequence: Failed to start GDB server

qcho.1
Associate II

Hi,

I wrote a code with stm32f407vg board on stm32cubeide.

There was no error in build, but when I run this program, there is error like title.

The full contents in error message is:

Error in final launch sequence:

Failed to start GDB server

Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (255) Unknown. Please check power and cabling to target.

It's connecting on my computer properly, and when I run other program a few days ago, It was work well.

How can I solve this problem?

Thanks for any answer.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

First check STLink with other sw utility or newer programmer. Use connect under reset.