cancel
Showing results for 
Search instead for 
Did you mean: 

Differences between Live Expressions and SWV

Mohammad A
Senior

What's the difference between Live Expressions and SWV Data Trace?

Are they both realtime?

Do both of them put a load on MCU processor?

Can I use Live Expressions with MCUs which do not provide SWO pin like CortexM0?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Markus GIRDLAND
ST Employee

Live Expressions does not require any specific peripheral in the MCU which means you can use it with Cortex-M0 while the SWV is required for SWV data trace.

Neither put any real load on the MCU processor.

SWV utilizes timestamps which gives more precise knowledge of when the memory access happened on the target device, live expressions doesn't.

SWV is limited to 4 memory addresses while Live Expression is in theory unlimited while adding many variables will cause slower periodic updates.

The main benefit of Live Expressions is that it's easy to set up and get started and that it works on any Cortex-M.

View solution in original post

4 REPLIES 4
Markus GIRDLAND
ST Employee

Live Expressions does not require any specific peripheral in the MCU which means you can use it with Cortex-M0 while the SWV is required for SWV data trace.

Neither put any real load on the MCU processor.

SWV utilizes timestamps which gives more precise knowledge of when the memory access happened on the target device, live expressions doesn't.

SWV is limited to 4 memory addresses while Live Expression is in theory unlimited while adding many variables will cause slower periodic updates.

The main benefit of Live Expressions is that it's easy to set up and get started and that it works on any Cortex-M.

Thank you. Your answer was perfect.

Mohammad A
Senior

But one last question, is it safe to use these debug methods in applications where timing is critical?

It's very precise so it should be. But I don't know the different demands that is required to be certified in different fields such as medical equipment etc.