cancel
Showing results for 
Search instead for 
Did you mean: 

Custom download location to avoid using SSD drive

EKarg.1
Associate

I am using STM32CubeIDE. It frequently downloads large files from internet (e.g.; device specific file when you start a new project, updates, etc).

The problem is, the files are downloaded to my C drive which is SSD. The download location is "C:\Users\<username>\STM32Cube\Repository".

I want to set this location to a custom one (for example somewhere in drive D) in order to save my SSD drives lifetime. How do I do this?

1 REPLY 1

Should be in the settings/options as well as being configurable when installing.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..