2025-05-07 3:14 AM
2025-05-07 3:23 AM
Hello @MichalPorazko
I've just tested on the STM32CubeIDE V1.18.1 and it works fine (as expected).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-08 3:33 AM
No I don't mean that its nor working in every version of the STM32CubeIDE V1.18.1, I m trying to figure it out if I maybe clicked something causing the ctrl + z to not work.
Now its suddenly working but I was wondering if there is some kind of setting which can be accidently turned off and hence also disabling the crlt + z command