cancel
Showing results for 
Search instead for 
Did you mean: 

Build Analyzer issue

matt-crc
Senior II

Hello,

Is there a trick to get the Build Analyzer to produce data every time the code is compiled?   It seems like the only way I can get it to update the window is if I change something in the linker script file and recompile again.   Is there an easier way or a setting that needs to be set?

thanks

Matthew

 

1 ACCEPTED SOLUTION

Accepted Solutions

@Mahmoud Ben Romdhane @TDK

Oops, I take that back... Mahmoud sent me a private email showing me the trick on how to get it to work each and every time... I've tested it 10 times now, and it seems to work for me.  Not sure why this trick is not public, so I will post the solution here...

after the user builds the project, you must right click on the project name, and select refresh.  Then the update for the building analyzer works.  Give it a try and let me know if it works for you too.  

 

View solution in original post

21 REPLIES 21
Pavel A.
Super User

PavelA_0-1741577029014.png

 

Hi @Pavel A. 

I just tried your suggestion, and when the "auto" is turned on, the refresh button is disabled:

mattcrc_0-1741577862074.png

turning off "Auto" re-enables that button, but I still have the original problem of the build analyzer not updating.

Either the build analyzer window is blank, or it is using data from an older compile.

Hello @matt-crc ,

First let me thank you for posting.

I suggest that you refer to UM2609, section 2.5 where this new button is explained and how you can change the behavior.

 

MahmoudBenRomdhane_1-1741592997517.png

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Mahmoud Ben Romdhane 

I figured out the button settings as per section 2.5 of your manual... But the main problem is getting the data.

In Auto Mode, the build analyzer does not update

in On Request mode, the build analyzer does not update with the refresh icon.

Do you know how to get the Build analyzer to work reliably?

@matt-crc ,

 

I suggest that you restart STM32CubeIDE, then build the project, knowing that I am using STM32CubeIDE 1.18.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

matt-crc
Senior II

@Mahmoud Ben Romdhane 

I'm running STM32cbutIDE 1.18 as well....  There must be a better way than having to restart the package after each compile....

matt-crc
Senior II
TDK
Super User

My experience: The behavior used to work but was broken some time in the past few updates. The "auto" refresh doesn't work, and while restarting stm32cubeide works (once), it's hardly a solution.

If you feel a post has answered your question, please click "Accept as Solution".
matt-crc
Senior II

@TDK @Mahmoud Ben Romdhane 

Yeah, its a real pain to have to restart the tool to check where the variables are stored