2025-02-19 4:28 AM
quite a useful extension, it's much better than 1.x, yet there are still garbled characters with progress bar of task "flash(SWD)", in a lot computers, the progress bar is "圹"&“北”. I solved it by add "chcp 437" to task "flash(SWD)" in "lauch.json", but to solve that perform permanently, sincerely expect you can change it in source code. Thanks in advance!!!
garbled
change encoding, yet temporarily solved
2025-03-25 3:40 AM
Hi @bonestan
will be fixed in a next release thanks a lot for the feedback