Skip to main content
Associate
April 22, 2024
Question

STM32 VScode undefined reference HAL_FLASH_Unlock

  • April 22, 2024
  • 3 replies
  • 3393 views

Hello everyone,

I am currently taking my first steps with the STM32VScode extension. Previously I worked exclusively with the STM32cubeIDE.

I created a Cmake project via STM32cubeMX, which I then imported via the STM32 VScode extension. Everything worked fine. The build process afterwards was successful and I was able to run the program on my Nucleo-C31C6 board.

Now I want to access the flash memory. But as soon as I insert the function HAL_FLASH_Unlock() into my code, the following error occurs during the build process: main.c:109: undefined reference to `HAL_FLASH_Unlock'.

How do I have to include the HAL drivers correctly so that I can use the function?

 

maxl95

3 replies

Andrew Neil
Super User
April 22, 2024

So do you have a definition for HAL_FLASH_Unlock anywhere in your project?

 


@maxl95 wrote:

How do I have to include the HAL drivers correctly so that I can use the function?


As with any C code:

  1. You need to #include the appropriate header(s) in the file(s) where you call the function;
  2. You need to have the source file(s) which define the function - ie, contain its executable body - in your Project.
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
maxl95Author
Associate
April 22, 2024

Hi Andrew, thanks for your quick replay,

  1. I've #include "stm32c0xx_hal_flash.h" in my main.c
  2. The source file is in the defaul directory --> ./Drivers/STM32C0xx_HAL_Driver/Src

I have also successfully used other functions (e.g. LL_USART) where the problem did not occur.

Andrew Neil
Super User
April 22, 2024

@maxl95 wrote:
  1.  
  2. The source file is in the defaul directory --> ./Drivers/STM32C0xx_HAL_Driver/Src

And is that file actually getting built?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Nawres GHARBI
ST Technical Moderator
April 25, 2024

Hello @maxl95 

Actually Flash drivers are by default integrated to your project

If you are adding HAL_FLASH_Unlock()  to a custom file you can include main.h or stm32c0xx_hal_conf.h to get flash functions available in your custom file

Visitor II
March 13, 2025

Hello @maxl95

I've just encountered this problem in my project but with STM32F4, and I'm also building with CMake. 

I've added the stm32f4xx_hal_flash.c path into my main CMakeLists.txt to PROJECT_SOURCES list along with files from Core/Src. And that works for me.