cancel
Showing results for 
Search instead for 
Did you mean: 

New STM32Cube for Visual Studio Code extension released (3.4.11)

Nawres GHARBI
ST Employee

 

 stm32.pngvscode.jfif

We are pleased to announce the new  STM32Cube for Visual Studio Code Extension Pack

 

The st-cube-code-pack extension for Visual Studio Code is designed to enhance the development experience for STM32 microcontrollers by providing a comprehensive and updatable set of tools. The *extension pack* allow users to install one single pack bringing a full STM32 IDE experience into VS Code.

 

Breaking Changes

  • Complete architecture redesign: The tool architecture has been split into three major building blocks with the purpose of creating a flexible, maintainable and updatable platform consisting of the following blocks: GUI, CLI tools and STM32 device support.
  • GUI: The platform's single extension has been transformed into an extension pack, offering a more modular, maintainable and flexible setup.
  • CLI tools: A new bundle manager is enabling VS Code to download required CLI tools. This replaces the all-in-one STM32CubeCLT package. The bundle manager will provide developers flexibility, updatability and re-producibility in terms of CLI tooling.
  • STM32 device support: The STM32 device support is decoupled from VS Code and sourced via CMSIS-PACK DFPs. Developers can now start using a new MCU without having to install a new STM32CubeCLT package.
  • Enhanced Debugging: A new, rich debugging experience is now available, leveraging a brand new STMicroelectronics-owned DAP (Debug Adapter Protocol) implementation, supporting both ST-LINK and SEGGER J-Link debug probes.
  • Clangd Integration: The update now relies on `clangd` for managing C/C++ code indexing, enhancing code navigation and analysis capabilities.
  • Auto-Discovery of STM32Cube Projects: This feature automatically detects STM32Cube projects, streamlining the setup and configuration process.

 

Pre-release (New!)

This release represents a major advancement in delivering a comprehensive and efficient VS Code-based development environment for STM32 microcontroller projects. ST is offering this version as a pre-release to set appropriate expectations. It introduces a new platform architecture that will serve as the basis for the evolving STM32Cube for VS Code environment. As with any innovative tool, it will undergo a maturation process. 

 

 Features

  • Project Creation Modes: Two distinct modes for project creation are supported, offering flexibility in development workflows:
    • STM32CubeMX Projects: Supports project creation with integrated CMake, enabling streamlined configuration and management.
    • Empty Projects: Allows for the creation of bare projects with CMake, providing a clean slate for custom development.
  • Build Analysis Solution: A new build analysis solution has been integrated, offering insights into build performance and optimization opportunities.
  • Board manager: The board manager view allows developers to show the ST-LINK serial number and update the ST-LINK firmware.
  • Enhanced RTOS debug: The existing open-source debug views have been complemented with two additional tree views showing additional kernel objects as well as the full call stack for all RTOS threads. Supported RTOSes are FreeRTOS and ThreadX.
  • Bundle Manager View: A dedicated view for managing bundles has been introduced, simplifying the management of project tool dependencies.
  • Cube CLI Command: The `cube` CLI command is now available, providing efficient tool management through command-line operations.

 

Documentation

The STM32Cube for VS Code extension offers a wealth of resources directly accessible within your integrated development environment. By installing the extension pack, you gain access to the "STM32Cube Resources" section, which is a centralized hub for valuable information which includes:

- Manuals: Comprehensive documentation that covers various aspects of STM32 development. These manuals provide detailed insights into the functionalities and features of STM32 microcontrollers, helping you understand the hardware and software integration.

- Tutorials: Step-by-step guides designed to assist both beginners and experienced developers. These tutorials cover a wide range of topics, from basic setup and configuration to advanced programming techniques, ensuring you have the guidance needed to effectively utilize STM32Cube tools.

 

Feedback & Support

If you need assistance or have any questions regarding STM32 for VS Code, support is readily available. You can access a wide range of resources and get help from the STMicroelectronics support team. Additionally, your feedback is valuable to us and helps improve the STM32 for VS Code extension. If you have any suggestions, issues, or comments, we encourage you to share them with the community.

- Feedback: To give feedback and participate in discussions, visit the [STM32 VS Code Extension Forum.](https://community.st.com/t5/stm32-vscode-extension-mcus/bd-p/stm32-vscode-extension-mcus)

- Community and ST expert help: To get help through our community and our ST experts on our forum, visit the [STM32 VS Code Extension Forum.](https://community.st.com/t5/stm32-vscode-extension-mcus/bd-p/stm32-vscode-extension-mcus)

- ST Support Home: For more information about getting support, visit the [STMicroelectronics Support Home.](https://www.st.com/content/st_com/en/support/support-home.html)

 

Download

https://marketplace.visualstudio.com/items?itemName=stmicroelectronics.stm32-vscode-extension

 

16 REPLIES 16
Peter3718
Associate III

coud you provide launch.json temple?  it's the key to launch a project successfuly.  Automatically generated launch.json only has few or worng information.  You can not assume new user know every fields.

Peter

Sounds weird to me to ask for some launch.json template what promoted extension(s) has(ve) to generate ...
I guess ST is not going to promote one to one launch.json ... up to them but ?

Instead could you point what sounds "wrong information" according to you .... if bug then a chance to get something back.
About "few" same please comment more ... "few" maybe sufficient in real : what do you think ?
"You can not assume new user know every fields" ... VSCode way of working according to me ... any debugger comes with integration (dedicated extension) whatever it is (Python, C/C++, ... STLink stuff) and end user way to access is always the same : a launch.json promoting sane default to be fine tuned or not and having extra control you can get Thanks editor auto-completion ... What may be helpful as extra is either / or documentation / GUI on top launch.json : what do you think here too ?
Any extra comment appreciated will help this community to progress (I'm part of :-))

Hollies
Associate II

Hollies_0-1749814423996.pngHollies_1-1749814445713.png

The text is not aligned.

JD25
Associate

Please consider addressing https://github.com/clangd/vscode-clangd/issues/687 and https://github.com/clangd/clangd/issues/108 issues. It is preventing efficient refactoring on Windows platform.

Custom "stm32cube-ide-clangd.arguments" value doesn't cover "arm-none-eabi-g++.exe", which used by CMake for "compile_commands.json" if I enable CXX support. "--query-driver" clangd option supports globs (https://github.com/llvm/llvm-project/issues/56623)

Also, it would be great to have HAL/LL and other libraries be available and well-behaved for inclusion as https://cmake.org/cmake/help/latest/module/FetchContent.html and/or git submodules.

 

 

SharonVEC
Associate II

As described, the new extension "replaces the all-in-one STM32CubeCLT package".
The CLT package allowed us to download an all-in-one solution for building in the cloud (a CI/CD environment). How will this flexibility be maintained here? Can we download the "cube" CLI without using VSCode?

StHo
Associate

Dear ST Team,

Is the STM32Cube for Visual Studio Code Extension solely intended for the VS Marketplace?
Previous iterations relied on Microsoft tools such as CMake, which made them unsuitable for use with VS Codium.

Is this still the case with the current version of the STM32Cube for VSCode Extension?
Are there any plans to support VS Codium the future?

I’d appreciate any insights you can share regarding your roadmap and future plans in this area.

Kind regards