cancel
Showing results for 
Search instead for 
Did you mean: 

Good afternoon. Thanks for the help. New problem. When debugging a project on STM32MP157A-DK1 in engineering mode, the program sends a request via COM3 instead of a request via STlinck(OpenOCD). See the photo. Sincerely, Alexander.

Vlaty.1
Senior
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @Vlaty.1​ 

Your screenshot looks normal.

ST-Link connection is also providing a Virtual COM port seen as COM3 on your PC.

But you can noticed the display is grey highlighting this is not taken into account for JTAG/SWD link (Engi mode)

Are you facing issues while debugging ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Good afternoon, Oliver. Thanks for the help. I know why ping doesn't work. There is no ping driver in the linux net directory. Sincerely, Alexander.:grinning_face: пт, 18 �?ент. 2020 г. в 11:04, ST Community :