2020-09-03 1:26 AM
call every 40mS :
static uint32_t count;
VIRT_UART_Transmit(cameraCommHandle.huart,(uint8_t *)&count,sizeof(count));
OPENAMP_check_for_message();
count++;
when i printing what i get in linux i got this:
39.99 ms: 262
40.00 ms: 263
40.01 ms: 264
40.00 ms: 265
40.00 ms: 266
39.99 ms: 267
40.00 ms: 268
40.01 ms: 266
40.00 ms: 270
40.00 ms: 271
39.99 ms: 272
40.00 ms: 1
40.01 ms: 274
40.00 ms: 1
40.00 ms: 276
39.99 ms: 277
40.00 ms: 278
and it repeat itself every 256 counts
i attached the c program that reads the serial and prints the what in UARt.
Solved! Go to Solution.
2020-09-07 7:39 AM
Hi, the issue was at the flags config. one of the flag was that to take the bytes as console.
2020-09-03 4:46 AM
one more test that i did : its prints 8bit counter with string and 16 bit of dummy.
root@stm32mp1-ground4-mx:/usr/csr/bin# ./read_trigger
971.24 ms: (104) 4 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.95 ms: (208) 5 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.96 ms: (312) 6 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
500.08 ms: (416) 7 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.91 ms: (520) 8 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
500.04 ms: (624) 9 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.96 ms: (728) 10 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
500.05 ms: (832) 11 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.96 ms: (936) 12 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
500.01 ms: (1040) 10 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
500.03 ms: (1144) 14 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.98 ms: (1248) 15 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.97 ms: (1352) 16 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
read 103 bytes instead of 104
500.04 ms: (1455) 97 0 - bcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.97 ms: (1559) 18 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
read 103 bytes instead of 104
500.02 ms: (1662) 97 0 - bcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
499.96 ms: (1766) 20 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
500.05 ms: (1870) 21 0 - abcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrstuvwxyzabcdefghijklmnopqrst
2020-09-07 7:31 AM
Hi @SMich.1
This is some hint I received from expert.
In your code it could be worth to add a check that "rien==4 " to confirm success of read().
Also you can start to implement with further trace using the dynamic debug framework :
echo -n 'file virtio_rpmsg_bus.c +p' > /sys/kernel/debug/dynamic_debug/control
You will get a trace for all messages received by A7, helping to narrowing down where the issue may come from
Hope it help,
Olivier
2020-09-07 7:39 AM
Hi, the issue was at the flags config. one of the flag was that to take the bytes as console.
2020-09-07 7:55 AM
Hi @SMich.1
Good news !
For reference could you please details further which flag you are talking about ?
Thx
Olivier