2023-09-20 12:51 PM
Hi, when I inserted keyboard/mouse to USB host port, nothing happened (log console) and this even cause usb host stop working then.
But when I inserted keyboard/mouse to a hub and connect this hub to usb host port, everything working fine.
The problem is only happened with hid (keyboard/mouse). When I used USB thumb drive, it works just fine, no need the hub.
The chip I used is STM32MP153 and this is custom build
Does anyone know why or any hint?
Thanks.
Solved! Go to Solution.
2023-09-21 12:03 PM
I got it working. Need to enable ochi driver in device tree.
2023-09-21 12:03 PM
I got it working. Need to enable ochi driver in device tree.
2024-03-05 2:24 AM
I have a similar error but in device mode, if I connect my board to the PC without HUB there are big chances that it wont work, but when I use a hub it always is recognise be the PC.
Which drive did you precisely enable and where? Can you load some screen captures?
Thanks in advance.