cancel
Showing results for 
Search instead for 
Did you mean: 

URLError trying to populate SDK with Flutter engine

Gencay
Associate III

I am trying to populate sdk with flutter engine and having the error: URLError(gaierror(-3, 'Temporary failure in name resolution')

Here is the github link of the flutter layer:

https://github.com/meta-flutter/meta-flutter

ERROR: flutter-engine-git-r0 do_install: ExpansionError('do_install', "\n    install -D -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/so.unstripped/libflutter_engine.so \\\n        /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/lib/libflutter_engine.so\n\n    if ${@bb.utils.contains('PACKAGECONFIG', 'desktop-embeddings', 'true', 'false', d)}; then\n        install -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/so.unstripped/libflutter_linux_gtk.so /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/lib\n    fi\n\n    install -D -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/flutter_embedder.h \\\n        /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/include/flutter_embedder.h\n\n    install -D -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/icudtl.dat \\\n        /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/icudtl.dat\n\n    # create SDK\n    install -D -m0755 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/clang_x64/gen_snapshot \\\n        /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/clang_x64/gen_snapshot\n\n    cd /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/flutter\n    echo `git rev-parse HEAD` > /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/engine.version\n    echo ${FLUTTER_ENGINE_REPO_URL} >> /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/engine.version\n    echo ${@get_flutter_sdk_version(d)} >> /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/flutter_sdk.version\n\n    cd /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image//usr/share/flutter\n    zip -r engine_sdk.zip sdk\n    rm -rf sdk\n", URLError(gaierror(-3, 'Temporary failure in name resolution')))
ERROR: Logfile of failure stored in: /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/temp/log.do_install.3657615
Log data follows:
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-graphics/fontconfig/fontconfig_2.13.1.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/meta-flutter/recipes-devtools/depot-tools/depot-tools-native_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-extended/zip/zip_3.0.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-support/curl/curl_7.82.0.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/quilt/quilt-native_0.67.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/pkgconfig/pkgconfig_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/python/python3_3.10.4.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-core/glibc/glibc_2.35.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-clang/recipes-devtools/clang/clang-cross_git.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-clang/recipes-devtools/clang/compiler-rt_git.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-clang/recipes-devtools/clang/libcxx_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-support/ca-certificates/ca-certificates_20211016.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-extended/pbzip2/pbzip2_1.1.13.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['fontconfig', 'depot-tools-native', 'zip-native', 'curl-native', 'quilt-native', 'pkgconfig-native', 'pseudo-native', 'python3-native', 'glibc', 'clang-cross-arm', 'compiler-rt', 'libcxx', 'ca-certificates-native', 'patch-native', 'pbzip2-native', 'gcc-runtime', 'zlib', 'util-linux', 'expat', 'freetype', 'libtool-native', 'xz-native', 'zlib-native', 'openssl-native', 'util-linux-libuuid-native', 'libffi-native', 'libnsl2-native', 'gdbm-native', 'readline-native', 'libtirpc-native', 'bzip2-native', 'ncurses-native', 'sqlite3-native', 'linux-libc-headers', 'clang-native', 'binutils-cross-arm', 'libgcc', 'attr-native', 'libcap-ng', 'ncurses', 'libpam', 'util-linux-libuuid', 'bash-completion', 'opkg-utils', 'libxcrypt', 'libpng', 'texinfo-dummy-native', 'gettext-minimal-native', 'perl-native', 'libedit-native', 'swig-native', 'cmake-native', 'binutils-native', 'libxml2-native', 'flex-native', 'gnu-config-native', 'cracklib', 'flex', 'libpcre-native', 'zstd-native', 'm4-native']
| DEBUG: Python function extend_recipe_sysroot finished
ERROR: Task (/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/meta-flutter/recipes-graphics/flutter-engine/flutter-engine_git.bb:do_install) failed with exit code '1'
 

 

Here is the complete error text:

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @Gencay​ 

Did you try to contact @Community member​  owner of the layer ?

Also, did you take care that you are using Kirkstone while AFAIK the layer is only available/tested for dunfell ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Joel
Associate II