cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157F-DK, Run the SDK installation Error and Try to run python with Linux or flash it

PMeth.3
Associate

I'd try to follow a step of Installing the SDK in Ubuntu (which is on Raspberry pi 4 Model B 4GB using 26GB SD card)

in step 4 Run the SDK installation script

I get an Error

Error: incompatible SDK installer! your host is aarch64 and this SDK was built for x86_64 hosts.

What does it mean and how can I fix it

The main goal of this project is to try to run python (with the library) on STM32MP157F-DK, I have two ideas

1. Follow the step and put it with .py instead of .c (no idea with install a library)

2. Install Linux in STM32MP157F-DK and run python on it (need some guild also)

So here I have 3 question

Thank STM for letting me ask a question here.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gregory PLANCHON
ST Employee

Hello @PMeth.3​ ,

I'm not sure to understand your problem, Python is already available on STM32.

Could you give me more details about what you want to do in order to understand the problem and be able to help you?

Regards,

Grégory 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.