cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157CAA3 LCD ili9881 coupling

MWoło.2
Senior III

Hi,

I try to couple LCD TFT ili9881c (mipi dsi 2 lanes interface) with stm32mp157caa3.

My custom driver seems to be loading correctly.

When I type lsmod I get

Module                  Size  Used by                                           
cfg80211              651264  0                                                 
usb_f_rndis            24576  2                                                 
u_ether                20480  1 usb_f_rndis                                     
libcomposite           49152  10 usb_f_rndis                                    
galcore               516096  2                                                 
panel_ilitek_ili9881c    20480  0                                               
dwmac_stm32            16384  0                                                 
stmmac_platform        20480  1 dwmac_stm32                                     
stm32_adc_core         20480  0                                                 
spi_stm32              24576  0                                                 
sch_fq_codel           20480  3                                                 
ip_tables              24576  0                                                 
x_tables               24576  1 ip_tables                                       
ipv6                  512000  42

Unfortunately, the display is not working, only the backlight is working.

I checked twice the dts and looks good, driver is loading well. I can't find anything with 'drm'. What I missed? Shall I add some additional driver in the kernel or something install in the roofs?

In the log, I can see only

[    0.079013] platform 5a000000.dsi: Fixing up cyclic dependency with 5a001000.display-controller

and

[   13.730531] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0

1 ACCEPTED SOLUTION

Accepted Solutions
MWoło.2
Senior III

I think I can close this topic. The real problem is related with display itself. STM32MP1x support only 2 lane displays. My display have 4 lane and it can't be reconfigured by software to 2 lane - missing access to IM pins. So I think mipi works but the display can't be handled by 2 lanes.

View solution in original post

19 REPLIES 19
Erwan SZYMANSKI
ST Employee

Hello @Michał Wołowik​ ,

Can you tell me on which linux version you are working on ? 5.10 or 5.15 (DV 3.1 or 4.1 ?)

You mentioned your "custom driver" for ili9881 panel. Does it mean that you did not take the one upstreamed under <linux_folder>/drivers//gpu/drm/panel/panel-ilitek-ili9881c.c ?

Can you also share your device tree ?

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWoło.2
Senior III

Hi Erwan,

I also measure clk and data lines, completely silent on all.

Here are my dts, defconfig and modified panel-ilitek-ili9881c.c

Latest Openstlinux 4.1 kernel 5.15.

I used the original driver but with my own initialization list and other parameters.

MWoło.2
Senior III

I also check other not modified drivers, the result is the same.

Nothing on the MIPI lines and in the log.

/* compatible = "winstar,WF50DTYA3MNG10", "ilitek,ili9881c"; */
		compatible = "raydium,rm68200";

 I think I missed something due I start designing dts from Cube Mx.

Hello @Michał Wołowik​,

Looking at your shared files, I do not see obvious issue that can explain your problem.

Are you working on a custom board or is it the stm32mp157c-dk2 board ?

Just to get a little bit more information, we can take a look at the following things:

  • adding drm.debug="0xff" in Linux Kernel command line to have complete traces of DRM, that can give us some tips (dmesg log level should be as high too to see the logs)
  • getting the cat /sys/kernel/debug/clk/clk_summary to check if dsi/ltdc cllks are well prepared and enabled.
  • getting the modetest -M stm output to check if the connectors etc.. are well recognized by the system.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWoło.2
Senior III

Hi Erwan,

I added logs in the attachment.

This is not DK2 it's my custom board.

In my previous version, I get some errors that the clock is invalid, etc. Here is nothing, it's strange to me.

BR Michal

Erwan SZYMANSKI
ST Employee

Hello @Michał Wołowik​ ,

Are you able to probe the different signals in entry of your panel ?

Do you see the pixel clock etc or nothing ?

Can you provide a full boot log file with "dmsg" command ?

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Michał Wołowik​ ,

Sorry for the DRM logs I was not really clear. In fact I would like to see the DRM logs at boot time.

You can enable it with adding "drm.debug=0x2" in the Linux commandline (0x2 will display drivers message only).

In ST deliveries, we can modify it on bootfs partition in extlinux.conf files.

For example, with my stm32mp157f-dk2 I will have:

root@stm32mp1:/boot/mmc0_extlinux# cat stm32mp157f-dk2_extlinux.conf
 
# Generic Distro Configuration file generated by OpenEmbedded
menu title Select the boot mode
MENU BACKGROUND /splash.bmp
TIMEOUT 20
DEFAULT OpenSTLinux
LABEL OpenSTLinux
        KERNEL /uImage
        FDTDIR /
        INITRD /uInitrd
        APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 drm.debug=0x2
LABEL stm32mp157f-dk2-a7-examples
        KERNEL /uImage
        FDT /stm32mp157f-dk2-a7-examples.dtb
        INITRD /uInitrd
        APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
LABEL stm32mp157f-dk2-m4-examples
        KERNEL /uImage
        FDT /stm32mp157f-dk2-m4-examples.dtb
        INITRD /uInitrd
        APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200

and at boot time, the following DRM traces are displayed:

[    0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 drm.debug=0x2
[    3.118656] [drm:ltdc_load] 
[    3.662669] [drm:ltdc_load] 
[    4.219836] [drm:ltdc_load] 
[    4.219954] [drm:ltdc_load] Bridge encoder:31 created
[    4.220011] [drm:ltdc_load] Bridge encoder:33 created
[    4.220201] [drm:ltdc_load] ltdc hw version 0x00010300
[    4.220839] [drm:ltdc_plane_create] plane:35 created
[    4.220869] [drm:ltdc_load] CRTC:37 created
[    4.220890] [drm:ltdc_plane_create] plane:38 created
[    4.220898] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    4.226124] [drm] Driver supports precise vblank timestamp query.
[    4.233250] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
[    9.915889] [drm:ltdc_crtc_mode_valid] clk rate target 29700000, available 29700000
[    9.945755] [drm:ltdc_crtc_mode_valid] clk rate target 29700000, available 29700000
[    9.945787] [drm:ltdc_crtc_mode_fixup] requested clock 29700kHz, adjusted clock 29700kHz
[    9.945799] [drm:ltdc_plane_atomic_check] 
[    9.945815] [drm:ltdc_plane_atomic_check] plane:35 fb:40 (480x800)@(0,0) -> (480x800)@(0,0)
[    9.945873] [drm:drv_runtime_resume] 
[    9.945882] [drm:ltdc_resume] 
[    9.945912] [drm:ltdc_crtc_mode_set_nofb] CRTC:37 mode:480x800
[    9.945923] [drm:ltdc_crtc_mode_set_nofb] Video mode: 480x800
[    9.945954] [drm:ltdc_crtc_mode_set_nofb]  hfp 98 hbp 98 hsl 32 vfp 15 vbp 14 vsl 10
[    9.945975] [drm:ltdc_encoder_mode_set] 
[    9.946107] [drm:dw_mipi_dsi_get_lane_mbps] pll_in 24000kHz pll_out 428000kHz lane_mbps 428MHz
[    9.958729] [drm:dw_mipi_dsi_mode_set] failed to wait phy lock state
[   10.015631] [drm:ltdc_plane_atomic_update] fb: phys 0xd2200000
[   10.015650] [drm:ltdc_crtc_enable_vblank] 
[   10.015686] [drm:ltdc_crtc_atomic_enable] 
[   10.814514] [drm:ltdc_encoder_enable] 
[   10.814534] [drm:dw_mipi_dsi_phy_power_on] 
[   15.845557] [drm:ltdc_crtc_disable_vblank] 

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWoło.2
Senior III

Hi Erwan,

drm boot log

root@stm32mp1-computer-lcd:~# dmesg | grep drm
[    0.000000] Kernel command line: root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw drm.debug="0x02" console=ttySTM0,115200
[    0.500555] [drm:ltdc_load] 
[    2.249006] [drm:ltdc_load] 
[    2.249178] [drm:ltdc_load] Bridge encoder:31 created
[    2.249483] [drm:ltdc_load] ltdc hw version 0x00010300
[    2.267527] [drm:ltdc_plane_create] plane:33 created
[    2.267605] [drm:ltdc_crtc_init] CRTC:37 created
[    2.267645] [drm:ltdc_plane_create] plane:38 created
[    2.278255] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
[    9.426142] systemd[1]: Starting Load Kernel Module drm...
[   10.745919] [drm:ltdc_crtc_mode_valid] clk rate target 54000000, available 54000000
[   10.792624] [drm:ltdc_crtc_mode_valid] clk rate target 54000000, available 54000000
[   10.792725] [drm:ltdc_crtc_mode_fixup] requested clock 54000kHz, adjusted clock 54000kHz
[   10.792754] [drm:ltdc_plane_atomic_check] 
[   10.792827] [drm:drv_runtime_resume] 
[   10.792863] [drm:ltdc_resume] 
[   10.792914] [drm:ltdc_crtc_mode_set_nofb] CRTC:37 mode:720x1280
[   10.792938] [drm:ltdc_crtc_mode_set_nofb] Video mode: 720x1280
[   10.792960] [drm:ltdc_crtc_mode_set_nofb]  hfp 48 hbp 48 hsl 9 vfp 12 vbp 12 vsl 5
[   10.793045] [drm:ltdc_encoder_mode_set] 
[   10.793146] [drm:dw_mipi_dsi_get_lane_mbps] pll_in 24000kHz pll_out 776000kHz lane_mbps 776MHz
[   10.807297] [drm:dw_mipi_dsi_mode_set] failed to wait phy lock state
[   10.867439] [drm:dw_mipi_dsi_phy_power_on] 
[   10.867508] [drm:ltdc_plane_atomic_update] plane:33 fb:42 (720x1280)@(0,0) -> (720x1280)@(0,0)
[   10.867575] [drm:ltdc_plane_atomic_update] fb: phys 0xc3900000
[   10.867615] [drm:ltdc_crtc_atomic_enable] 
[   11.257293] [drm:ltdc_encoder_enable] 
[   11.257376] [drm:ltdc_crtc_enable_vblank] 
[   16.317225] [drm:ltdc_crtc_disable_vblank] 
[   18.130419] [drm:ltdc_plane_atomic_check] 
[   18.130532] [drm:drm_atomic_helper_commit_planes] CRTC:37 plane:33
[   18.130579] [drm:ltdc_crtc_enable_vblank] 
[   23.197261] [drm:ltdc_crtc_disable_vblank] 
[   27.588309] [drm:ltdc_crtc_mode_valid] clk rate target 54000000, available 54000000
[   27.695429] [drm:ltdc_plane_atomic_check] 
[   27.695491] [drm:ltdc_plane_atomic_check] 
[   27.749367] [drm:ltdc_plane_atomic_check] 
[   27.749426] [drm:ltdc_plane_atomic_check] 
[   27.749556] [drm:ltdc_plane_atomic_update] plane:33 fb:42 (720x1280)@(0,0) -> (720x1280)@(0,0)
[   27.749634] [drm:ltdc_plane_atomic_update] fb: phys 0xce400000
[   27.749669] [drm:ltdc_crtc_enable_vblank] 
[   29.098611] [drm:ltdc_plane_atomic_check] 
[   29.343705] [drm:ltdc_plane_atomic_check] 
[   29.343911] [drm:ltdc_plane_atomic_update] plane:33 fb:43 (720x1280)@(0,0) -> (720x1280)@(0,0)

full log in the attachment.

BR Michal

MWoło.2
Senior III

Hi Erwan,

unfortunately, I have nothing on dsi lines completely silent.

Please check my ioc, I have a feeling I missed something.

Thanks

BR Michal