Skip to main content
MPier.2
Associate
July 30, 2020
Solved

STM32MP157C-DK2 How to use external power supply?

  • July 30, 2020
  • 4 replies
  • 1890 views

I would like to provide power from PI connector. How to avoid error blocking message at the start of the boot that report:

***********************************************

* ERROR USB TYPE-C connection in unattached mode  *

* Check that USB TYPE-C cable is correctly plugged *

*    Current too low, use a 3A power supply!    *

***********************************************

This topic has been closed for replies.
Best answer by PatrickF

Hi,

We did not recommend using Arduino or GPIO expansion connectors to feed 5V to the DK1/DK2 board. the 5V_VIN power routing is not be guaranteed for 3A.

Furthermore, you will probably need to remove Q1 and Q2 to disconnect Type-C VBUS.

If you still want to do that at your own risk, you could remove the warning by choosing one of this 'hack':

  • SW: remove this check from the source code
  • HW : fake that a Type-C 3A supply is present by connecting a pull-up on one of the CC line (only one).
    • According to USB Type-C standard, you must use either 10 kΩ ± 5% to 4.75 – 5.5 V (e.g. VBUS) or 4.7 kΩ ± 5% to 3.3 V ± 5% (e.g. VDD). Please not that once this is done, I did not recommend to plug anymore an USB Type-C charger (not sure if any side effect of such hack)

Regards.

4 replies

PatrickF
PatrickFBest answer
ST Employee
July 30, 2020

Hi,

We did not recommend using Arduino or GPIO expansion connectors to feed 5V to the DK1/DK2 board. the 5V_VIN power routing is not be guaranteed for 3A.

Furthermore, you will probably need to remove Q1 and Q2 to disconnect Type-C VBUS.

If you still want to do that at your own risk, you could remove the warning by choosing one of this 'hack':

  • SW: remove this check from the source code
  • HW : fake that a Type-C 3A supply is present by connecting a pull-up on one of the CC line (only one).
    • According to USB Type-C standard, you must use either 10 kΩ ± 5% to 4.75 – 5.5 V (e.g. VBUS) or 4.7 kΩ ± 5% to 3.3 V ± 5% (e.g. VDD). Please not that once this is done, I did not recommend to plug anymore an USB Type-C charger (not sure if any side effect of such hack)

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
MPier.2
MPier.2Author
Associate
July 30, 2020

Thanks for the quickly answer.

We would like to use external power only to make a prototype, then we are ready to design our carrier board with the SOM.

For HW solution its clear.

For SW solution, I found on U-Boot source the file stm32mp1.c with function named "board_check_usb_power(void)". What need I do? Force to "return 0" on line 402?

PatrickF
ST Employee
July 31, 2020

Looking at the code, I propose to replace on line 462

		/* with 125ms interval, led will blink for 17.02 years ....*/
		nb_blink = U32_MAX;

by something like

		/* with 125ms interval, led will blink for 17.02 years ....*/
		nb_blink = 4;

So, the message is still there, but after 4 red led blinks (instead of 2^32 blinks !), the boot will continue.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
allard
Senior
November 3, 2020

I too want to connect a external power supply. My application is fairly low-power, so it should be OK with the DK2. I tried the HW solution 10K from CC1 to VBUS, but somehow I did not get rid of the message. How do I apply the SW solution to the distrubution package? Do i need to make a .patch file or a .bbappend?

EDIT: HW solution works now, 10K should be connected to 5v_IN, not VBUS.