cancel
Showing results for 
Search instead for 
Did you mean: 

HOW TO EXTERNAL POWER SUPPLY TO STM32MOU157X-DK2 BOARD

Charan28
Associate

Hi,

I’m using the STM32MPU157x-DK2 development board and would like to power it externally, either using a battery or a different power source (not USB Type-C).

Could you please help with the following:

  1. What are the recommended ways to provide external power, such as via a Li-ion/LiPo battery or regulated 5V supply?

  2. Can I use the 5V input on the CN6 (EXP connector) to power the board?

  3. Should I disconnect USB-C when supplying external power to avoid conflict?

  4. Are there any voltage/current limitations, or specific battery protection requirements I should consider?

  5. Do I need to change any configuration settings on the board to enable external power or battery supply?

 

1 REPLY 1
PatrickF
ST Employee

Hi @Charan28 

 

Board was not designed for battery powering (not low power optimization, no 1.8V IOs support, etc...)

 

CN6 (USB-C) must be used to supply the board with 5V supply (4V minimum).

In case your supply is not USB-C compliant, some errors might occurs (red led flashing and potentially stopped boot). To overcome this, you could remove this line from the uBoot Device Tree.

   		st,adc_usb_pd = <&adc1 18>, <&adc1 19>;

 

You must not supply the board from CN2 nor CN16 (power integrity issue, too weak wires, etc...).

 

Maybe best option is to use USB power bank.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here