Solved
STM32MP151C SPI5 clock much slower
- January 2, 2024
- 2 replies
- 1961 views
I am trying to configure SPI5 on STM32MP151C where MPU is a master and ESP32C6 is a slave. The clock used in the device tree is HSI 64MHz. SPI driver is running with 2MHz configured and divisor in the SPI_CFG1 register is correctly set to 32. In the dmesg logs I could see that speed is set to 2MHz.
What is actually measured with oscilloscope on a clk out is approximately a 1/1000 of configured frequency, around 1.8 kHz. Furthermore duty cycle is clearly not a 50%.
Would appreciate any ideas what might be wrong. Could it be some other function configured on that same pin used for clock? Problem in the device tree?