STM32MP135 TF-A SLC_NAND
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-27 2:42 AM
My hardware:
STM32MP135FAE SLC NAND(MT29F4G08ABAF):256MB page:4K block:256K
excuse me,How to configure makefile.sdk when compiling TF-A?
Here's what I tried:
# Init default config settings
TF_A_DEVICETREE_nand ?= stm32mp135f-dk
TF_A_EXTRA_OPTFLAGS_nand ?= STM32MP_RAW_NAND=1 PSA_FWU_SUPPORT=1 STM32MP_FORCE_MTD_START_OFFSET=0x00200000
TF_A_BINARY_nand ?= tf-a
TF_A_MAKE_TARGET_nand ?= all
-----------------------------------------------------------------
FlashLayout_sdcard_stm32mp135f-dk-optee.tsv
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0 tf-a-stm32mp135f-dk-usb.stm32
- 0x03 fip-boot FIP none 0x0 fip-stm32mp135f-dk-optee.bin
P 0x04 fsbl Binary nand0 0x00000000 tf-a-stm32mp135f-dk-nand.stm32
P 0x05 fsbl Binary nand0 0x00080000 tf-a-stm32mp135f-dk-nand.stm32
PE 0x06 metadata1 Binary nand0 0x00100000 metadate.bin
PE 0x07 metadata2 Binary nand0 0x00180000 metadate.bin
PE 0x08 fip-a1 FIP nand0 0x00200000
PE 0x09 fip-a2 FIP nand0 0x00600000
PE 0x0A fip-b1 FIP nand0 0x00a00000
PE 0x0B fip-ab2 FIP nand0 0x00e00000
PE 0x10 UBI System nand0 0x01200000
-----------------------------------------------------------------------------------
When I download to nand and BOOT was configured (b0:1 b1:1 b2:0), the FA-T could not be started and there was no output from the serial port. What I refer to is mp157,I think what details are not paid attention to,The MP135 might be a little differen, leading to abnormal startup
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-27 2:46 AM
I have tried:
uboot.dts
nand-ecc-strength = <1>;
nand-ecc-step-size = <512>;
or
nand-ecc-strength = <4>;
nand-ecc-step-size = <512>;
and
nand-ecc-strength = <8>;
nand-ecc-step-size = <512>;
None of this will solve the problem