STM32MP135 ADC buffer enable fails
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-04-13 3:54 AM
Hi, I am encountering some issues while trying to configure the ADC DMA Buffer on the STM32MP135 board , when I execute the following:
echo 1000 > /sys/bus/iio/devices/iio:device1/buffer/length
echo 1 > /sys/bus/iio/devices/iio:device1/scan_elements/in_voltage0_en
echo 1 > /sys/bus/iio/devices/iio:device1/buffer/enable
I receive the following error after the third command:
sh: write error: Invalid argumet
But when reading the ADC's raw output directly via:
cat /sys/bus/iio/devices/iio:device1/in_voltage0_raw
I am able to obtain a normal reading, which suggests that the basic functionality of the ADC is intact.
Operating System: 5.15.24 #1 PREEMPT Sat Apr 13 15:11:38 CST 2024 armv7l GNU/Linux
- Labels:
-
ADC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-04-15 11:51 PM
I have used the TIM trigger to operate the ADC in triggered buffer mode successfully.
However, the issue arises when I set the trigger frequency to high values, such as 1MHz.
cd /sys/bus/iio/devices/trigger0
echo 1000000 > sampling_frequency
I've noticed that the CPU usage spikes significantly, even the activation of RT Throttling and occurrences of RCU stalls.
I wonder if there are better ways to optimize this issue when using ADC buffer mode. How to use ADC continuous conversion mode without intervention from the CPU?
Thanks