cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157A DDR size detected wrong

jhi
Senior

I have a running system (based on bootlin buildroot) with kernel 5.10 and I wanted to update it to use the latest 6.1 and now I have a problem that the BL2 panics:

 

 

NOTICE:  CPU: STM32MP157AAC Rev.Z
NOTICE:  Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
NOTICE:  BL2: v2.8-stm32mp1-r1.0(release):custom()
NOTICE:  BL2: Built : 12:30:08, Apr 11 2024
ERROR:   DDR size: 0x10000000 does not match DT config: 0x20000000
PANIC at PC : 0x2ffeae01

 

 

The board is custom and it has 512MB. Any ideas?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
jhi
Senior

Never mind. I forgot to update the DDR settings (stm32mp15-mx.dtsi) for tfa.

View solution in original post

1 REPLY 1
jhi
Senior

Never mind. I forgot to update the DDR settings (stm32mp15-mx.dtsi) for tfa.