2024-06-19 5:49 AM
Currently, I am testing QuadSPI.
Is it correct for the output to include Command / Address / Data?
I want to output only Data. While I can remove the Address through settings, I couldn't remove the Command.
Is it possible to output only Data?
2024-06-20 8:05 AM
Hi @SL1
QUADSPI is build to interface external Flash or similar.
For you concern, did you try playing with IMODE setting ?
Regards
2024-06-25 9:00 PM
Hi, I recently solved this problem.
After checking, it was due to the ClockMode in the code below.
When I changed that part to XSPI_CLOCK_MODE_0, it worked correctly.
Is it correct that if it is set to XSPI_CLOCK_MODE_3, the address should be output before the data is output?
I will finish the post after confirming the answer.