2025-12-12 2:20 AM
Hello,
I'm working with a STM32MP257D, which is using the I2C-driver "i2c-stm32f7.c" in the Linux kernel (compatible: st,stm32mp25-i2c). I'm using kernel version v6.6.78.
I need to use I2C mangling, specifically I2C_M_NOSTART and I2C_M_STOP, to handle a receiving master scenario.
My specific situation: I'm communicating with a device that sends the length of the data payload in the third byte of the transmission. This means I need to:
1. Read the first 3 bytes to get the length information
2. Continue reading the remaining data without sending a STOP condition after the initial 3-byte read
3. Continue reading without sending a START condition when fetching the remaining data
Code Example:
struct i2c_msg xfer[2];
xfer[0].addr = addr;
xfer[0].flags = I2C_M_RD | I2C_M_STOP;
xfer[0].len = 0x03;
xfer[0].buf = buff;
ret = i2c_transfer(i2c->adapter, xfer[0], 1);
xfer[1].addr = addr;
xfer[1].flags = I2C_M_RD | I2C_M_NOSTART;
xfer[1].len = buff[2];
xfer[1].buf = &buff[3];
ret = i2c_transfer(i2c->adapter, xfer[1], 1);Questions:
From investigating the driver I know that using I2C_M_STOP / I2C_M_NOSTART isn't supported.
- Is there an existing patch or workaround for this use case?
- Has anyone encountered a similar situation and found a solution?
- Is it even possible with this device?
Any guidance would be greatly appreciated!
Best regards
Manuel
2026-01-26 1:54 AM
Hello,
I would really appreciate an answer. I can't imagine that it's not possible to use I2C-mangling. That it's not possible to have more access to the i2c protocol. Or is the hardware not capable of it?
Thank you in advance.
Best regards
Manuel