poweroff command line issue
- September 15, 2021
- 5 replies
- 3506 views
Hello ST Teams!
We're testing another one stm32MP1 custom board (battery powered), and i've issue with poweroff command line function:
Each time i use this function, board is rebooting instead of poweroffing (...)
With these info from tfa:
INFO: Reset reason (0x814):
INFO: Pad Reset from NRST
I've see a similar post on ST Forum, but it doesn't help me!
We are using a STM32MP1 from your Octavo partner, and i will post on their forum too.
Octavo have encapslulated STM32MP1+PMIC+DDR on a single chip, so PMIC should be correctly wired.
We have a PONKEY wired on the board, witch works perfectly, i can shutdown and wakeup by an action on "power" button.
I've tried lot of distribution configuration, looked at PMIC internal registry, but i've no hints on what cause this.
I've tried to use a "generic" Octavo Distribution (BRK one), stopped booting at uboot, to avoid unnecessary software issue, but i've the same behaviour.
I'm feeling that there is an hardware issue, but i don't see where it is?
May someone give me an advice on this problem?
have a nice day!