cancel
Showing results for 
Search instead for 
Did you mean: 

New : STM32MP15 distribution for Android™ v1.0.0

Olivier GALLIEN
ST Employee

ST is please to announce the st-android-9.0.0-2019-09-27 tag compatible with Android 9.0.0 (Pie).

Main software component versions :

·       Android version v9.0.0 (AOSP android-9.0.0_r46 tag)

·       Kernel version v4.19.49 (AOSP common kernel) + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       TF-A version v2.0 + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       U-Boot version v2018.11 + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       OP-TEE version v3.3.0 + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       STM32CubeMP1 FW v1.1.0

·       GCC version v8.2

·       openOCD version v0.10.0

·       GCnano version v6.2.4

ST want to warn that this delivery is provided as demonstrator/enabler with following limitation/restriction :

-       No Android CTS/VTS qualification

-       No performance optimization

-      Productization only through partner

The recommended configuration:

   Display @480p

    DDR32bit 1GB

 The STM32MP15X-EVAL includes by default a display @720p, which has impacts on performances.

Customer should not expect same level of performance than with an OctoCore at 2Ghz + High end GPU .

The Andoid AOSP aim to make application in adequation with platform usage target (typically not smartphone UI like application)

Production is only supported by our partner program: (https://www.st.com/content/st_com/en/partner/partner-program/partnerpage.html.

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0