STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I enable LinuxPTP PPS Output?

I know that to get PPS output on the Ethernet PPS Pin PG8 that the device tree has to configure the pin for AF11. I also believe that PPS has to be enabled somehow? ​On some embedded Linux systems there is a /sys/class/ptp/ptp0/pps_enable variable to...

Issue with OPTEE driver on version 3.9.0

Hello,Our team is currently working on stm32mp1 boards (the dk2 and the ev1).Our software architecture is using TFA, OPTEE, Uboot and Linux.For our needs, we have developed an SPI driver for OPTEE. The OPTEE version on which we developed this driver ...

romain2 by Associate III
  • 1132 Views
  • 0 replies
  • 0 kudos

Traininigs STM32MP1

We are searching for a training possiblity on the MP1 processor, which is in Germany. Mainly we are interested in the HW and the software e.g. multiprozessor handling. There are online courses but they do not deep dive. Anyone an idea about this? ST ...

JMein.1 by Associate III
  • 1997 Views
  • 2 replies
  • 0 kudos

Resolved! usage of i2c read command in U-Boot

Hi,I have a custom board with a ST32MP157C and a 24AA025E48 on a i2c bus.In the U-Boot, I want to read the MAC address located in the 24AA025E48 on the i2c bus 1 at address 0x53 at offset 0xFA.When I can use the following commands it works (MAC Addre...

TJann.1 by Associate II
  • 3165 Views
  • 2 replies
  • 0 kudos

Resolved! Mistake in STM32MP1-DK2 schematics?

Hi all.The en.MB1272-DK2-C01_Schematic.pdf states thatARD_A0 : PF14 -> ADC1_IN0ARD_A1 : PF13 -> ADC1_IN1ARD_A2 : ANA0 -> ADC2_IN6ARD_A3 : ANA1 -> ADC2_IN2I've spend quite some time to figure out that this is wrong and the correct pinout is:ARD_A0...

dimtass by Associate II
  • 2088 Views
  • 1 replies
  • 2 kudos