2019-08-18 08:00 AM
How long does it take (approx) to rise or lower a GPIO pin fix configured to the M4 in the STM32MP157c, after issuing the command in the M4 code ? On our native STM32F409 board it takes around 10ns. I'm afraid the STM32MP1xx is much slower right ?
Regards,
Daniel
2019-08-20 05:48 AM
Hi @DB.7uergin
Once a GPIO is allocated to M4 context there is no difference driving a GPIO from an MP1 M4 or STM32F4.
So no reason for a specific overhead here.
Did you measure something different to make this assumption ?
Br,
Olivier
2019-08-20 11:54 AM
Hi Oliver
Ok thanks that sounds good. No i didn't measure anything on the MP1 Board, but i've made some bad experiences with other boards (i.MX7dual) where the GPIOs are quite slow (150 - 200ns) to raise or lower.
So it should be enough to lock my GPIO with "PERIPH_LOCK()" inside the M4 at the beginning of my code or do i need to update the DeviceTree ? I'm not sure if i already understood the ways of allocating the resources to either side (A7 or M4) 🙂
But anyway thanks for the answer.
Daniel