cancel
Showing results for 
Search instead for 
Did you mean: 

Is UEFI implementation documented/detailed ?

bhstalel
Associate

Hello,

I read the STM32MP boot process in this link.

And it is a generic Embedded Linux boot process (ROM, SPL, Uboot, Kernel).

But, when I read further about STM32MP I figured out that U-boot UEFI commands are enabled, and there is support for PXE network boot which is supported from UEFI environment which is in this case executed from U-boot. Also I found a GPT support on flash memories (eMMC, ..).

I'm asking is there a documentation about UEFI on STM32MP ? Like:

  • Is it optional ? (Can it be disabled ?)
  • Is there support for EDK and UEFI application development ?
  • Is UEFI boot process documented ?

Thanks,

Talel

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0