cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying to integrate OPTEE with one of my custom Yocto distro. I have an STM32MP157f -dk2 eval board. I have added optee in machine conf and disto conf files. It build successfully but the raw image on sd card has uboot failure. Need help

KMark.1
Associate II

I followed some of the steps to integrate OPTEE with Yocto builds as below.

meta-bsp-stm32mp1/conf/machine/stm32mp157f.conf

MACHINE_FEATURES +="optee"

BOOTSCHEME_LABELS += "optee"

meta-product-stm32mp157x-dk2/conf/distro/pxred-stm32mp1-dk2.conf - distro changes

DISTRO_FEATURES_append = " px-red-kinit-e2fsprogs \

                            optee \ "

The following is the boot message I get on terminal

NOTICE: CPU: STM32MP157FAC Rev.Z

NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board

NOTICE: Board: MB1272 Var4.0 Rev.C-02

INFO:  Reset reason (0x15):

INFO:   Power-on Reset (rst_por)

INFO:  PMIC version = 0x20

INFO:  Using SDMMC

INFO:   Instance 1

INFO:  Boot used partition fsbl1

NOTICE: BL2: v2.2-r2.3(debug):v2.2-dirty

NOTICE: BL2: Built : 08:34:06, Apr 17 2022

INFO:  Using crypto library 'stm32_crypto_lib'

INFO:  BL2: Doing platform setup

INFO:  RAM: DDR3-DDR3L 16bits 533000Khz

INFO:  Memory size = 0x20000000 (512 MB)

INFO:  BL2 runs OP-TEE setup

INFO:  BL2: Loading image id 4

INFO:  Loading image id=4 at address 0x2ffc0000

INFO:  STM32 Image size : 512

INFO:  Image id=4 loaded: 0x2ffc0000 - 0x2ffc0200

WARNING: Skip signature check (header option)

NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.

INFO:  OPTEE ep=0x2ffc0000

INFO:  OPTEE header info:

INFO:     magic=0x4554504f

INFO:     version=0x2

INFO:     arch=0x0

INFO:     flags=0x0

INFO:     nb_images=0x2

INFO:  BL2: Loading image id 21

INFO:  Loading image id=21 at address 0x2ffc0000

INFO:  STM32 Image size : 68960

INFO:  Image id=21 loaded: 0x2ffc0000 - 0x2ffd0d60

WARNING: Skip signature check (header option)

NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.

INFO:  BL2: Loading image id 22

INFO:  Loading image id=22 at address 0xde000000

INFO:  STM32 Image size : 233472

INFO:  Image id=22 loaded: 0xde000000 - 0xde039000

WARNING: Skip signature check (header option)

NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.

INFO:  BL2: Loading image id 5

INFO:  Loading image id=5 at address 0xc0100000

INFO:  STM32 Image size : 904892

INFO:  Image id=5 loaded: 0xc0100000 - 0xc01dcebc

WARNING: Skip signature check (header option)

NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.

NOTICE: BL2: Booting BL32

INFO:  Entry point address = 0x2ffc0000

INFO:  SPSR = 0x1d3

I/TC: Early console on UART#4

I/TC:

I/TC: Pager is enabled. Hashes: 1920 bytes

I/TC: Pager pool size: 112kB

I/TC: No non-secure external DT

I/TC: Embedded DTB found

I/TC: OP-TEE version: 3.9.0-dev (gcc version 9.3.0 (GCC)) #1 Sun Apr 17 08:35:13 UTC 2022 arm

I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp157f-dk2.dts

I/TC: DT clock tree configurations were ignored

I/TC: DTB enables console (non-secure)

I/TC: Initialized

U-Boot 2020.01-stm32mp-r2.2 (Apr 17 2022 - 08:21:32 +0000)

CPU: STM32MP157FAC Rev.Z

Model: STMicroelectronics STM32MP157F-DK2 Discovery Board

Board: stm32mp1 in trusted mode (st,stm32mp157f-dk2)

Board: MB1272 Var4.0 Rev.C-02

DRAM: 512 MiB

Clocks:

- MPU : 800 MHz

- MCU : 208.878 MHz

- AXI : 266.500 MHz

- PER : 24 MHz

- DDR : 533 MHz

WDT:  Started with servicing (32s timeout)

NAND: 0 MiB

MMC:  STM32 SD/MMC: 0, STM32 SD/MMC: 1

Loading Environment from MMC... *** Warning - bad CRC, using default environment

In:  serial

Out:  serial

Err:  serial

Net:  eth0: ethernet@5800a000

Hit any key to stop autoboot: 0

** Unrecognized filesystem type **

Wrong Image Format for bootm command

ERROR: can't get kernel image!

My Flashlayout file generated has following sections

#Opt  Id   Name  Type  IP   Offset Binary

-    0x01  fsbl1-boot   Binary none  0x0   arm-trusted-firmware/tf-a-stm32mp157f-dk2-serialboot.stm32

-    0x03  ssbl-boot    Binary none  0x0   bootloader/u-boot-stm32mp157f-dk2-optee.stm32

P    0x04  fsbl1  Binary mmc0  0x00004400   arm-trusted-firmware/tf-a-stm32mp157f-dk2-optee.stm32

P    0x05  fsbl2  Binary mmc0  0x00044400   arm-trusted-firmware/tf-a-stm32mp157f-dk2-optee.stm32

PD   0x06  ssbl  Binary mmc0  0x00084400   bootloader/u-boot-stm32mp157f-dk2-optee.stm32

PD   0x0A  teeh  Binary mmc0  0x00284400   optee/tee-header_v2-stm32mp157f-dk2-optee.stm32

P    0x0B  teed  Binary mmc0  0x002C4400   optee/tee-pageable_v2-stm32mp157f-dk2-optee.stm32

P    0x0C  teex  Binary mmc0  0x00344400   optee/tee-pager_v2-stm32mp157f-dk2-optee.stm32

P    0x21  boot  System mmc0  0x00384400   st-image-bootfs-pxred-stm32mp1-dk2-stm32mp157f.ext4

P    0x22  vendorfs    FileSystem   mmc0  0x04384400   st-image-vendorfs-pxred-stm32mp1-dk2-stm32mp157f.ext4

P    0x23  rootfs FileSystem   mmc0  0x05384400   px-red-image-stm32mp157f.ext4

P    0x24  userfs FileSystem   mmc0  0x33D84400   st-image-userfs-pxred-stm32mp1-dk2-stm32mp157f.ext4

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0