Question
How to Wake up STM32MP157AAD3 from LPLV-Stop mode?
Our board is similar to STM32MP157C-DK2 Disco board - All the Developer packages has been installed, At the initial FSBL stage itself board is not booting whereas required power supply is provided, In which the Voltage (VDDCORE_1V2) value related to DDR circuit has fallen below Threshold voltage to 0.88V , so the voltages related to it has also went down to 0v. What is the solution to wake up the MPU ?