2021-10-19 10:55 AM
EDIT: Found the solution, read for implementation
I'm trying to get the MPU to exit from standby.
PWR_ON goes to 0 as expected on shutdown, so far so good.
I'm using PA2 (WKUP2) but it's not working at all...
Is there anything special to setup in the device tree?
I am using discrete power supplies as instructed in the app notes. (PWR_ON to enable pins)
Here's my dts config for TF-A
&pwr_regulators{
status = "okay";
secure-status = "okay";
/* USER CODE BEGIN pwr_regulators */
system_suspend_supported_soc_modes = <
STM32_PM_CSLEEP_RUN
STM32_PM_CSTOP_ALLOW_LP_STOP
STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR
>;
system_off_soc_mode = <STM32_PM_CSTOP_ALLOW_STANDBY_DDR_OFF>;
/* USER CODE END pwr_regulators */
};
Linux config part
wkup {
compatible = "gpio-keys";
#address-cells = <1>;
#size-cells = <0>;
autorepeat;
status = "okay";
button@2 {
label = "WakeUp2";
linux,code = <BTN_1>;
interrupts-extended = <&exti_pwr 56 IRQ_TYPE_EDGE_RISING>; // PA2
status = "okay";
wakeup-source;
};
};
Thank you
Solved! Go to Solution.
2021-10-26 7:51 AM
The issue was the missing gpio-key (it's not documented...)
I've added it in the original post.
2021-10-25 3:17 AM
Any ideas?
2021-10-26 7:51 AM
The issue was the missing gpio-key (it's not documented...)
I've added it in the original post.
2021-10-27 12:42 AM
Hi @fpoussin ,
Well catch ! We will work to enhance documentation related to Wake Up.
For next time, please avoid using edit of original post and provide solution in comment.
Thx
Olivier