STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Whitepaper: Protecting OEM assets and ensuring firmware integrity through STM32 and open-source solutions

Learn how to protect OEM assets and ensure integrity using open-source softwareDownload our whitepaper to better understand these strategies:Secure Boot: How it works and why it is importantHow chain-of-trust mechanisms protect OEM and user dataSecur...

0693W00000KaZJ6QAN.png

STM32MP157C-DK2 board boot at panic mode

I flashed the board with dd command and tried either flashing whole SD card with the .raw image and each partition separately as well, it came up at panic mode. The image is en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0. Does any...

DZ.2 by Associate II
  • 3868 Views
  • 8 replies
  • 0 kudos

Resolved! STM32MP157C qspi nand flas w25n512 using

Hi,I am using stm32mp157c and working initialize mtd nand flash w25n512. I am following the https://wiki.st.com/stm32mpu/wiki/MTD_overview . I don't have choise "Support most SPI Flash chips (AT26DF, M25P, W25X, ...)" in chapter 3.1.2 in my kernel me...

aliMesut by Associate III
  • 3040 Views
  • 2 replies
  • 0 kudos

Hardware: STM32MP1-DK1 Software: Windows STM32Cube Programmer Question: Download hardware failed.

Hardware: STM32MP1-DK1Software: Windows STM32Cube ProgrammerQuestion: Download hardware failed. NOTICE: CPU: STM32MP157AAC Rev.B NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board NOTICE: Board: MB1272 Var1.0 Rev.C-01 INFO: Reset...

0693W00000JPeAlQAL.png
李放.1 by Associate II
  • 2386 Views
  • 3 replies
  • 0 kudos

Resolved! How do I build this example project?

When I hit the build button, I get "Nothing to build for project DK2_TIMER1_OpenAmp_Solution", the Debug folder is also empty, should this be populated or do I need to generate it somehow?https://www.youtube.com/watch?v=PsiFDHH87vo&list=PLnMKNibPkDnF...

msche.1 by Associate III
  • 1883 Views
  • 4 replies
  • 0 kudos