cancel
Showing results for 
Search instead for 
Did you mean: 

Error trying to build dtb

OHaza.1
Associate III

Hi, I tried to follow the example in the youtube workshop, moving a pwm timer to the a7 side. I was able to create a dts file with cube mx but when running make to build the dtb i get

"reference to non existent node or label "ethernet_mac_address""

Is it possibly some mismatch between versions of cube and the openst dist?

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @OHaza.1​ ,

>> Is it possibly some mismatch between versions of cube and the openst dist?

Refer to wiki release note to check consistency between OpenST version and tools

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OHaza.1
Associate III

Ok, thanks, looks like things have changed in the last few days/weeks, so could well be that.