cancel
Showing results for 
Search instead for 
Did you mean: 

DK1 examples list?

OHaza.1
Associate III

Hi is there a list, or sorts, with the examples that should work for the DK1 dev board from the DK2 examples?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @OHaza.1​ ,

DK1 differ from DK2 only with absence of on-board screen and no Wifi+Bluetooth chipset.

So from the DK2 supported exemple list in "STM32Cube_FW_MP1_V1.2.0/Projects/STM32CubeProjectsList.html" I see only the "AI_Character_Recognition" which is limited without screen.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.