2020-10-26 7:46 AM
We would like to build the TF-A image with a different muxer setting
for i2c4. The usual setting is:
i2c4_pins_a: i2c4-0 {
pins {
pinmux = <STM32_PINMUX('Z', 4, AF6)>, /* I2C4_SCL */
<STM32_PINMUX('Z', 5, AF6)>; /* I2C4_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
our setup:
i2c4_pins_a: i2c4-0 {
pins {
pinmux = <STM32_PINMUX('H', 11, AF6)>, /* I2C4_SCL */
<STM32_PINMUX('H', 12, AF6)>; /* I2C4_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
If we use the changed pin muxing we get no signal output on those pins.
My question, is it possible to change the pin muxing
or is the muxing for I2C4 fixed for the TF-A build ?
Solved! Go to Solution.
2020-10-26 11:49 PM
Hello Olivier,
after updating the TF-A firmware to version v2.2-r1.4 the problem
is solved.
I think the reason was the issue:
"GPIO clock not enabled in BL32"
thank you,
Ralf
2020-10-26 7:57 AM
Hi @RGlie.1
I suspect you are facing known GPIO clock issue in V2.0.
Olivier
2020-10-26 11:49 PM
Hello Olivier,
after updating the TF-A firmware to version v2.2-r1.4 the problem
is solved.
I think the reason was the issue:
"GPIO clock not enabled in BL32"
thank you,
Ralf