cancel
Showing results for 
Search instead for 
Did you mean: 

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution Why?

Vlaty.1
Senior

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution Why? What did I do wrong? Sincerely, Alexander

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @Vlaty.1​ 

Can you better explain what you are trying to achieve ?

ttyRPMSG0 is used to exchange message/data between A7 and M4.

From where did you try to connect with ssh-t ttyRPMSG0 ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Good morning. Thanks for the help. But when trying to contact stm32mp157a-DK1 (), there is no communication channel again. Device on com 3, idle/busy status .Address 192.163.1.7 once green . This usually worked stably. Sincerely, Alexander. пн, 26 окт. 2020 г. в 19:23, ST Community :