cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP2 does not have USB OTG - SD card is the only option then?

DMårt
Lead

At STM32MP1, there is an USB OTG, were you can flash the eMMC via the USB OTG. 

But in STM32MP2, there is no USB OTG. Does this mean that I need to flash my SD-card instead? Just like Raspberry Pi etc.?

Or am I supposed to flash the eMMC via the USB C connector?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

HI @DMårt 

in STM32MP2, USB3DR IP is the equivalent of OTG seen on STM32MP1.

You flashload using USB type-C or USB micro-B in same way.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

HI @DMårt 

in STM32MP2, USB3DR IP is the equivalent of OTG seen on STM32MP1.

You flashload using USB type-C or USB micro-B in same way.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here