cancel
Showing results for 
Search instead for 
Did you mean: 

BSP_EXIT_CRITICAL_SECTION for I2C5 init code for CM4 in STM32MP1

PVaaz.1
Associate III

Hello,

For generating the I2C5 init code, I took the I2C4 discovery kit example and modified it accordingly.

Unlike in I2C4, I see the banks of the I2C_DATA and I2C_CLK are different

I2C5: ( GPIOz and GPIO D)

0693W00000NqxMMQAZ.pngfor I2C4 (GPIOZ):

0693W00000NqxMRQAZ.pngin the I2C4 code generation, there was this critical section code which is present around the CLK and DATA , since in I2C4 both the gpio banks are same, there was this code,

 /* Configure I2C Tx, Rx as alternate function */

 gpio_init_structure.Pin = DISCO_I2C4_SCL_PIN | DISCO_I2C4_SDA_PIN;

 BSP_ENTER_CRITICAL_SECTION(DISCO_I2C4_SCL_SDA_GPIO_PORT);

 HAL_GPIO_DeInit(DISCO_I2C4_SCL_SDA_GPIO_PORT, gpio_init_structure.Pin);

 BSP_EXIT_CRITICAL_SECTION(DISCO_I2C4_SCL_SDA_GPIO_PORT);

but for I2C5 does it has to be changed for both the GPIO Banks of CLock and data?Is it mandatory?

Please advice.

Best,

Ped

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @PVaaz.1​ ,

BSP_ENTER_CRITICAL_SECTION is an abstraction to Periph_Lock / HSEM.

It prevent simultaneous access from A7 and M4 world at same time.

It's recommended to apply it properly

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.