cancel
Showing results for 
Search instead for 
Did you mean: 

Time of erase after a tamper

FAlca.1
Associate II

Hi all,

I am using MPU ref. STM32MP153F, do you say me what is the time that elapsed between a tamper is detected and the backup resister are finishing erased?

And the backup SRAM?

Thank you in advance

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @Community member​ ,

Reference Manual answer to your questions.

Erase event is generated with the following latency:

  • 3 ck_apre cycles when TAMPFLT differs from 0x0 (level detection with filtering)
  • 3 ck_apre cycles when TAMPTS = 1 (timestamp on tamper event)
  • No latency when TAMPFLT = 0x0 (edge detection) and TAMPTS = 0

Note that active tamper has obviously additional latency as clocked transitions.

Backup registers are erased immediately on erase event (let's says few ten of ns).

The backup RAM is not mass erased by an tamper event, instead it is read protected to prevent confidential data, from being accessed.

To regain access to the backup RAM after a tamper event, it needs to be first erased. (e.g. SW must write zero on the whole memory).

RAM.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hi @Community member​ ,

Reference Manual answer to your questions.

Erase event is generated with the following latency:

  • 3 ck_apre cycles when TAMPFLT differs from 0x0 (level detection with filtering)
  • 3 ck_apre cycles when TAMPTS = 1 (timestamp on tamper event)
  • No latency when TAMPFLT = 0x0 (edge detection) and TAMPTS = 0

Note that active tamper has obviously additional latency as clocked transitions.

Backup registers are erased immediately on erase event (let's says few ten of ns).

The backup RAM is not mass erased by an tamper event, instead it is read protected to prevent confidential data, from being accessed.

To regain access to the backup RAM after a tamper event, it needs to be first erased. (e.g. SW must write zero on the whole memory).

RAM.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here