cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1waking from Standby by WAKE UP pins

AKudr.1
Associate II

Hello everyone!

I’ve tested wake up from standby mode with Wake up pins PI11 (and PI8). But it is not work 

I have remove all definitions about wake up pins in dts except place where it defines as wake up pins in stm32mp151.dtsi 

Entering in standby mode by putting ‘echo mem > /sys/power/state’. And after that MPU no wakes by I acting on pins PI11 or PI8.

I do not see any WAKE UP Pins in /sys/kernel/debug/wakeup_sources, maybe I need activate it before going to standby?

Do I need set MPU_BEN bit in RCC_MP_BOOTCR before going to standby mode? If yes — how?

Maybe another my misunderstanding?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
OlivierK
ST Employee

Hello AKudr.1 (Community Member) 

In fact IRQ EXTI from 55 to 60. are respectively connected to wkup pin 1 to 6. These wakeup pins are hardcoded. you can refer to the Datasheet they are respectively

             wakeup-gpios = <&gpioa 0 GPIO_ACTIVE_HIGH>, 

                                      <&gpioa 2 GPIO_ACTIVE_HIGH>,

                                      <&gpioc 13 GPIO_ACTIVE_HIGH>,

                                      <&gpioi 8 GPIO_ACTIVE_HIGH>,

                                      <&gpioi 11 GPIO_ACTIVE_HIGH>,

                                      <&gpioc 1 GPIO_ACTIVE_HIGH>;

IRQ EXTI 55 corresponds to PA0, IRQ EXTI 56 to PA2, etc..

Therefore to use PI8 and PI11 you need to use respectively in your DT:

interrupts-extended = <&exti_pwr 58 IRQ_TYPE_EDGE_FALLING>;  

interrupts-extended = <&exti_pwr 59 IRQ_TYPE_EDGE_FALLING>;  

The corresponding driver need to use the IRQ EXTI. As an example driver you can use "gpio-keys"

/

...

test_wkup {

        compatible = "gpio-keys";

        #address-cells = <1>;

        #size-cells = <0>;

        autorepeat;

        status = "okay";

        button@4 {

              label = "WakeUp4";

              linux,code = <BTN_1>;

              interrupts-extended = <&exti_pwr 58 IRQ_TYPE_EDGE_FALLING>;

              status = "okay";

              wakeup-source;

        };

};

root@stm32mp1:~# cat /sys/kernel/debug/wakeup_sources              

name      active_count  event_count   wakeup_count  expire_count  e

test_wkup    5        5        0        0       0

10000000.m4   0        0        0        0       0

mmc1      0        0        0        0       0

mmc0      0        0        0        0       0

5c002000.i2c:stpmic@33:onkey  0        0        0       0

alarmtimer.0.auto    0        0        0        0   0

5c004000.rtc  0        0        0        0       0

deleted     0        0        0 

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
OlivierK
ST Employee

Hello AKudr.1 (Community Member) 

In fact IRQ EXTI from 55 to 60. are respectively connected to wkup pin 1 to 6. These wakeup pins are hardcoded. you can refer to the Datasheet they are respectively

             wakeup-gpios = <&gpioa 0 GPIO_ACTIVE_HIGH>, 

                                      <&gpioa 2 GPIO_ACTIVE_HIGH>,

                                      <&gpioc 13 GPIO_ACTIVE_HIGH>,

                                      <&gpioi 8 GPIO_ACTIVE_HIGH>,

                                      <&gpioi 11 GPIO_ACTIVE_HIGH>,

                                      <&gpioc 1 GPIO_ACTIVE_HIGH>;

IRQ EXTI 55 corresponds to PA0, IRQ EXTI 56 to PA2, etc..

Therefore to use PI8 and PI11 you need to use respectively in your DT:

interrupts-extended = <&exti_pwr 58 IRQ_TYPE_EDGE_FALLING>;  

interrupts-extended = <&exti_pwr 59 IRQ_TYPE_EDGE_FALLING>;  

The corresponding driver need to use the IRQ EXTI. As an example driver you can use "gpio-keys"

/

...

test_wkup {

        compatible = "gpio-keys";

        #address-cells = <1>;

        #size-cells = <0>;

        autorepeat;

        status = "okay";

        button@4 {

              label = "WakeUp4";

              linux,code = <BTN_1>;

              interrupts-extended = <&exti_pwr 58 IRQ_TYPE_EDGE_FALLING>;

              status = "okay";

              wakeup-source;

        };

};

root@stm32mp1:~# cat /sys/kernel/debug/wakeup_sources              

name      active_count  event_count   wakeup_count  expire_count  e

test_wkup    5        5        0        0       0

10000000.m4   0        0        0        0       0

mmc1      0        0        0        0       0

mmc0      0        0        0        0       0

5c002000.i2c:stpmic@33:onkey  0        0        0       0

alarmtimer.0.auto    0        0        0        0   0

5c004000.rtc  0        0        0        0       0

deleted     0        0        0 

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AKudr.1
Associate II

Thanks you very much. Now I realized how it works. 

---

But unfortunately I faced another problem with device trees. I found in tf-a output after waking from STANDBY this strings:

ERROR: Illegal access to 0xe0000000 in :

ERROR:   Non-Secure

ERROR:   Privilege

ERROR:   Read

But this is another story for another forum thread)