cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157AAD3 , SD-Card Booting is not working?

JG.2
Associate II

Our board is similar to STM32MP157C-DK2 Disco board - All the Developer packages has been installed, the board is not booting whereas required power supply is provided, All the Test Points and passive components on the Board shows their desired Voltages.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
PatrickF
ST Employee

Hi,

please have a look to

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview#Debug_and_error_cases

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_trace_analyzer

and maybe also

How to configure U-Boot for your board

How to create your board device tree

As you are trying to boot from SD-Card, could we assume your other posts are resolved ?

How to Wake up STM32MP157AAD3 from LPLV-Stop mode?

What is the reason for Rapid increase of Temperature in STM32MP157AAD3?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hi,

No the issue is not yet Resolved. we need some more links or support to do .

As other issues you mention in other posts are likely highlighting an HW issue on your board (shortcut, wrong connections, etc...), I think you should first resolve those one before going to boot trials.

Once you are able to do some ROM Traces (link in previous reply) on a stable HW, please share them if you need more insight on analysis.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here