cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP153 fip works from sdcard not when loaded through programmer

lorenzoruffati
Associate

I have a system (built using yocto kirkstone) working with the bootchain TF-a -> sp_min -> uboot when loaded from the sdcard and from the emmc

I have tried to boot into uboot by loading it directly into memory (as a precondition to the use it to flash the emmc) by following this guide: https://wiki.st.com/stm32mpu/wiki/How_to_load_U-Boot_with_STM32CubeProgrammer

I have used the correct tf-a binary and it does manage to load SP_MIN (I get all the SP_MIN traces), but the boot just hangs afterwards.

Does u-boot require some special compilation flag in order to be used in this manner?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi @lorenzoruffati ,

Could you share

  • the command line you are using with CubeProgrammer
  • the .TSV file
  • the complete cubeprogrammer log
  • the complete board serial console log

Did you hit CTRL+C on the board serial console to get the uBoot prompt ?

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here