cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 M4 programming

STrat.1
Associate

Hi,

Currently i am looking for an easy way:

to change the device tree, to assign peripherals to the M4 Coprocessor for quasi real time applications.

i do have a STM32MP157F-DK2 board for testing and also a board with Debian, which i purchased from a different vendor who has built it´s own Linux image, which i want to use.

The vendor does not provide any CubeMX files for his design, or any other information regarding his design.

So... do i need to built everything from scratch myself ?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @STrat.1​ 

For DK2 board for sure you can use CubeMX to generate DTS assigning peripherals to M4.

Can you please give the reference of the other board you are talking about ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ste_Trat1
Associate

Hi,

here is the topic creator once again.

The problem:

i stopped some time ago with this and now more people are interested in resolving this.

 The reference board is, which can enter production or engineering mode.

https://www.olimex.com/Products/OLinuXino/STMP1/STMP157-OLinuXino-LIME2/open-source-hardware

to which i sucessfully connected with st link and got some response of the board.

olimex has its own image called Olimage, and has a guide to change the device tree blob:

https://raw.githubusercontent.com/OLIMEX/OLINUXINO/master/DOCUMENTS/OLIMAGE/Olimage-guide.pdf

Goals:

Extract the information to generate an ioc file for cubemx to built my own STlinux Yocto image.

or

simply program the M4 core with .elf files, for realtime tasks and i do not want the A7 to interfere somewhow with the M4 through shared resources. They should work independently from each other and only communicate via remoteproc.

How can i accomplish this?

 

Thanks & BR