cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 ECO Unused GPIO busy after gpioset

debugging
Lead

Kernel tree does not assign any driver to pin PZ2. After gpioset -c gpiochip11 2=1, the pins goes actually high (from low) but the gpioset program stalls. SSH at that moment into the device shows:

 

line 0: "PZ0" input
line 1: "PZ1" input
line 2: "PZ2" output consumer="gpioset"
line 3: "PZ3" input
line 4: "PZ4" input consumer="kernel"
line 5: "PZ5" input consumer="kernel"
line 6: "PZ6" input
line 7: "PZ7" input

 

Aborting CTRL-C/Z gpioset causes the device to be busy upon a next set.

Is there a way to set the pin and the client release itself as consumer of  GPIO pin to be able to change the pin later back to low?

 

root@stm32mp1:~# gpioset -c gpiochip11 2=1
^Z[1]+ Stopped gpioset -c gpiochip11 2=1
root@stm32mp1:~# gpioset -c gpiochip11 2=0
gpioset: unable to request lines on chip '/dev/gpiochip11': Device or resource busy

root@stm32mp1:~# gpioget -c gpiochip11 2
gpioget: unable to request lines: Device or resource busy

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @debugging 

according to https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace, it is needed to use CTRL+C (and not CTRL+Z which keep the gpioset process running in background, which block further ressource usage). I don't know why gpioset is working like that.

To force exit of gpioset immediately, you need to use '-t0'

gpioset -t0 -c gpiochip11 2=1

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

3 REPLIES 3
PatrickF
ST Employee

Hi @debugging 

according to https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace, it is needed to use CTRL+C (and not CTRL+Z which keep the gpioset process running in background, which block further ressource usage). I don't know why gpioset is working like that.

To force exit of gpioset immediately, you need to use '-t0'

gpioset -t0 -c gpiochip11 2=1

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
debugging
Lead

Tank you very much.  this helps a lot. Perhaps good to add to the wiki.

wiki update is planned even if the listed CTRL+C works and this is more a libgpio v2 specificity (seems an intended behavior).
I think it is minor as only command line issue. In an application, behavior is more clean.

regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here