Running DDR_Init on STM32MP135F-DK board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-13 5:47 AM - edited ‎2024-09-04 3:09 AM
Hi all,
i'm trying to run the DDR_Init project as my first project on STM32MP135F-DK board.
I loaded the project on CDT Eclipse IDE and added some configurations: the build is ok.
I report the main.c compiler command line as example:
Building file: C:/Progetti/dbTechnologies/testSTM32/DDR/Projects/STM32MP135C-DK/Examples/DDR/DDR_Init/Src/main.c Invoking: GNU Arm Cross C Compiler arm-none-eabi-gcc -mcpu=cortex-a7 -mthumb -mfloat-abi=hard -mfpu=vfpv4-d16 -Og -ffunction-sections -fstack-usage -g3 -DCORE_CA7 -DUSE_STM32MP13XX_DK -DSTM32MP135Fxx -DDDR_TYPE_DDR3_4Gb -I"C:\Progetti\dbTechnologies\testSTM32\DDR\Drivers\CMSIS\Device\ST\STM32MP13xx\Include" -I"C:\Progetti\dbTechnologies\testSTM32\DDR\Drivers\CMSIS\Core_A\Include" -I"C:\Progetti\dbTechnologies\testSTM32\DDR\Drivers\BSP\STM32MP13xx_DISCO" -I"C:\Progetti\dbTechnologies\testSTM32\DDR\Projects\STM32MP135C-DK\Examples\DDR\DDR_Init\Inc" -I"C:\Progetti\dbTechnologies\testSTM32\DDR\Drivers\STM32MP13xx_HAL_Driver\Inc" -std=gnu11 -MMD -MP -MF"Application/User/main.d" -MT"Application/User/main.o" -c -o "Application/User/main.o" "C:/Progetti/dbTechnologies/testSTM32/DDR/Projects/STM32MP135C-DK/Examples/DDR/DDR_Init/Src/main.c" Finished building: C:/Progetti/dbTechnologies/testSTM32/DDR/Projects/STM32MP135C-DK/Examples/DDR/DDR_Init/Src/main.c
The commandline for linker is:
Building target: DDR_Init_A7.elf Invoking: GNU Arm Cross C Linker arm-none-eabi-gcc -mcpu=cortex-a7 -mthumb -mfloat-abi=hard -mfpu=vfpv4-d16 -Og -ffunction-sections -fstack-usage -g3 -T "../stm32mp13xx_a7_sysram.ld" -Xlinker --gc-sections -Wl,-Map,"DDR_Init_A7.map" --specs=nano.specs --specs=nosys.specs -static -o "DDR_Init_A7.elf" ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_ddr.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_dma.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_dma_ex.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_gpio.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_i2c.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_pwr.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_pwr_ex.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_rcc.o ./Drivers/STM32MP13xx_HAL_Driver/stm32mp13xx_hal_rcc_ex.o ./Drivers/CMSIS/irq_ctrl_gic.o ./Drivers/CMSIS/mmu_stm32mp13xx.o ./Drivers/CMSIS/system_stm32mp13xx_A7.o ./Drivers/BSP/STM32MP13xx_DISCO/stm32mp13xx_disco.o ./Drivers/BSP/STM32MP13xx_DISCO/stm32mp13xx_disco_bus.o ./Drivers/BSP/STM32MP13xx_DISCO/stm32mp13xx_disco_stpmic1.o ./Application/User/main.o ./Application/User/stm32mp13xx_hal_msp.o ./Application/User/stm32mp13xx_it.o ./syscalls.o C:/Program Files (x86)/Arm GNU Toolchain arm-none-eabi/13.3 rel1/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: cannot find entry symbol Reset_Handler; not setting start address Finished building target: DDR_Init_A7.elf
When I upload the binary on board by GDB OpenOCD Debug profile, the run breaks with the message:
Break at address "0x4904" with no debug information available, or outside of program code.
I don't think this is the main() entry point ..
If I press 'Resume F8' button the program seems to continue, and the red LED is steady on - the USB STLink LED is flashing red/green.
I also added some other breakpoints (in the main function and others) but none of them breaks.
Am I missing some compiler options? Or they are wrong?
Thanks!
Solved! Go to Solution.
- Labels:
-
STM32MP13 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-23 2:17 AM
Hi @SteMMo ,
ST highly recommend to use CubeIDE for an optimal experience.
Can you try with it and come back if issue still present ?
Thanks
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-15 12:30 AM
Maybe I solved downgrading the toolchain from 13.3 to 12.3 (??)
I'm investigating ...
Anyone knows issues on gnu arm gcc relase 13.3 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-23 2:17 AM
Hi @SteMMo ,
ST highly recommend to use CubeIDE for an optimal experience.
Can you try with it and come back if issue still present ?
Thanks
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-09-03 7:34 AM
Ok, finally I moved to CubeIDE, I found toolchain 12.3 and evething works,
Thanks