2021-05-11 7:47 AM
Hi All -
I was attempting to build the Qt example images for the DK2, following the wiki directions here:
https://wiki.st.com/stm32mpu/wiki/How_to_build_and_use_an_SDK_for_QT
I got to the step where it's building the SDK, after compiling the image successfully.
PC $> bitbake st-example-image-qt -c populate_sdk
And got a compile error:
arm-ostl-linux-gnueabi/9.3.0/ld: .obj/moc_qgeotiledmaplabs_p.o:(.data.rel.ro+0x70): undefined reference to `QGeoTiledMap::setCopyrightVisible(bool)'
| /home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/recipe-sysroot-native/usr/bin/arm-ostl-linux-gnueabi/../../libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/9.3.0/ld: .obj/moc_qgeotiledmaplabs_p.o:(.data.rel.ro+0x80): undefined reference to `QGeoTiledMap::clearScene(int)'
| /home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/recipe-sysroot-native/usr/bin/arm-ostl-linux-gnueabi/../../libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/9.3.0/ld: .obj/moc_qgeotiledmaplabs_p.o:(.data.rel.ro+0x84): undefined reference to `QGeoTiledMap::evaluateCopyrights(QSet<QGeoTileSpec> const&)'
| collect2: error: ld returned 1 exit status
| make[2]: *** [Makefile:774: ../../lib/libQt5Location.so.5.14.2] Error 1
| make[2]: Leaving directory '/home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/build/src/location'
| make[1]: *** [Makefile:181: sub-location-make_first] Error 2
| make[1]: Leaving directory '/home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtlocation/5.14.2+gitAUTOINC+feb604c326_d9577fdebe-r0/build/src'
| make: *** [Makefile:49: sub-src-make_first] Error 2
| WARNING: exit code 1 from a shell command.
|
And this summary:
Summary: 1 task failed:
/home/mtd/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-qt5/recipes-qt/qt5/qtlocation_git.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Help?
Solved! Go to Solution.
2021-08-17 3:48 AM
Hi @Jean-Marc B , This is the log of my operation:
DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
bitbake st-example-image-qt -c populate_sdk
Initialising tasks: 100% |#########################################################################################################################################################################################################################################| Time: 0:00:07
Sstate summary: Wanted 325 Found 318 Missed 7 Current 1994 (97% match, 99% complete)
NOTE: Executing Tasks
ERROR: qtconnectivity-5.14.2+gitAUTOINC+b445ea4ff2-r0 do_compile: oe_runmake failed
ERROR: qtconnectivity-5.14.2+gitAUTOINC+b445ea4ff2-r0 do_compile: Execution of '/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/temp/run.do_compile.2711' failed with exit code 1:
cd src/ && ( test -e Makefile || /home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/recipe-sysroot-native/usr/bin/qmake -o Makefile /home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/git/src/src.pro QT_BUILD_PARTS-=examples QT_BUILD_PARTS-=tests ) && make -f Makefile
make[1]: Entering directory '/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/build/src'
cd bluetooth/ && ( test -e Makefile || /home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/recipe-sysroot-native/usr/bin/qmake -o Makefile /home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/git/src/bluetooth/bluetooth.pro QT_BUILD_PARTS-=examples QT_BUILD_PARTS-=tests ) && make -f Makefile
cd nfc/ && ( test -e Makefile || /home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/recipe-sysroot-native/usr/bin/qmake -o Makefile /home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/git/src/nfc/nfc.pro QT_BUILD_PARTS-=examples QT_BUILD_PARTS-=tests ) && make -f Makefile
make[2]: Entering directory '/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/build/src/nfc'
rm -f libQt5Nfc.so.5.14.2 libQt5Nfc.so libQt5Nfc.so.5 libQt5Nfc.so.5.14
linking ../../lib/libQt5Nfc.so.5.14.2
make[2]: Entering directory '/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/qtconnectivity/5.14.2+gitAUTOINC+b445ea4ff2-r0/build/src/bluetooth'
rm -f libQt5Bluetooth.so.5.14.2 libQt5Bluetooth.so libQt5Bluetooth.so.5 libQt5Bluetooth.so.5.14
linking ../../lib/libQt5Bluetooth.so.5.14.2
……
ERROR: Task (/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-qt5/recipes-qt/qt5/qtcharts_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6448 tasks of which 6446 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 35 seconds
Summary: 2 tasks failed:
/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-qt5/recipes-qt/qt5/qtconnectivity_git.bb:do_compile
/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-qt5/recipes-qt/qt5/qtcharts_git.bb:do_compile
Summary: There were 4 ERROR messages shown, returning a non-zero exit code.
2021-08-17 8:17 AM
Hi @枭 陈
I don't see any compilation or link errors in your log. I think the log output is cut (the …… in your previous post) and that hides the interesting messages.
Could you make another attempt please by attaching the log output (use the paper clip symbol available when writing a reply).
Best regards,
--JM
2021-08-17 9:41 AM
Hi @Jean-Marc B
I rebuilt the SDK and recorded all build logs。
2021-08-17 11:48 PM
Hi @枭 陈
Thank you for the ouput log. I will analyze them soon and keep you posted.
Best regards,
--JM
2021-08-18 2:44 AM
Hello @枭 陈
I can't explain the many «undefined references» from your output log. I just make an attempt on a machine running ubuntu 18 and the following commands:
$ rm -rf build-openstlinuxeglfs-stm32mp1
$ DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
$ bitbake qtconnectivity
$ bitbake qtchartsBoth recipes are successfully built.
Could you give me your OS environment please?
Could you try to re-do the whole process from scratch so the bitbake cache is empty? I suspect a mismatch between versions in Yocto cache.
Best regards,
--JM
2021-08-18 9:57 AM
Hi @Jean-Marc B(ST Employee)
My host uses a virtual machine environment built by VMware, as follows:
Windows 10, 64-bit :Intel(R) Core(TM) i9-10850K CPU @ 3.60GHz 3.60 GHz, RAM 16.0 GB
VMware® Workstation 15 Pro 15.5.0 + ubuntu-20.04.2.0(CPU:4*2, RAM:8G)
I am trying:
$ rm -rf build-openstlinuxeglfs-stm32mp1
$ DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
$ bitbake qtconnectivity
$ bitbake qtcharts
and
Both $ bitbake qtconnectivity and $ bitbake qtcharts executed successfully.
So I continue to execute:
PC $> bitbake st-example-image-qt is executed successfully.
Then I execute:
PC $> bitbake st-example-image-qt -c populate_sdk
Currently still under construction, the following error has occurred:
ERROR: Task (virtual:native:/home/cx/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-qt5/recipes-qt/qt5/qt3d_git.bb:do_compile) failed with exit code '1'
I execute :
$ bitbake qt3d
Error still exists。
I want to know your build environment, whether it is the linux host or the linux environment on the virtual machine, and the corresponding version, I will use it as a reference.Or can you recommend a software version built on a virtual machine environment for me to experiment?
2021-08-19 2:02 AM
Hi @枭 陈
The build of st-example-image-qt is fine with my different configurations (ub16 native, zoostrap running ub18 or running ub20).
Is the error you mention with the recipe qt3d related to some «undefined references» too?
If you run these commands:
$ bitbake -c cleansstate qt3d
$ bitbake qt3dis the error still here?
Maybe there are some «bad» items in the yocto cache. Did you share the locations defined by the variables SSTATE_DIR or SSTATE_MIRRORS (defined in conf/local.conf and conf/site.conf) with someone else or with different yocto environments?
Best regards,
--JM
2021-08-21 9:09 AM
Hi @Jean-Marc B(ST Employee)
Like the previous error, the error mentioned in the recipe qt3d is related to some "undefined reference".
I ran the following command:
$ bitbake -c cleansstate qt3d
$ bitbake qt3d
error still exists.
My build started in a brand new environment, and I can't determine the "bad" items in the Yocto cache.
At present, I completely replaced the original build environment, used virtualbox6.1.26, and downloaded the VDI file Ubuntu 20.04.2 (64bit)VDI from osboxes.org according to "PC prerequisites." in the wiki.
Both $bitbake st-example-image-qt and $bitbake st-example-image-qt -c populate_sdk were executed successfully.
PC $> bitbake st-example-image-qt is executed successfully.
PC $> bitbake st-example-image-qt -c populate_sdk is executed successfully.
Very happy and thank you for communicating with you a few days ago.
2021-08-23 12:11 AM
Hi @枭 陈
thank you for your feedback! I am happy you finally solve your problem.
Best regards,
--JM