cancel
Showing results for 
Search instead for 
Did you mean: 

Succesfully bringup STM32MP135 with FMC NAND

EricD-IES
Associate

Hi,

 

Just now I have done bringing up a custom board for STM32MP133/ STM32MP135 with OpenST Linux, with kernel 6.2:

- The whole boot chain bring up from tf-a, uboot, kernel.

- Configure PMIC and support DDR test.

- Support FMC NAND, change flash partition layout.

- A/B FOTA ready Yocto build (with uboot)

- Total boot time is 30 seconds to access to ADB (android platform tool)

- Platform CAN bringup

- Integrate Quectel modem for network over LTE

If someone needs something related to this, I can help.

Best,

Eric

 

0 REPLIES 0