cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to use UART1 in STM32MP135F-DK board

SteMMo
Senior

Hi all,

I own a STM32MP135F-DK board and  started to write a simple firmware on it based on RTX threads.

I'd like to use USART1 port as simple terminal interface with the board.

I chose USART1 cause it is present on CN8 connector (RX + TX) and cause the UART8 presents only TX pin.

The code I wrote is:

 

 

void MX_USART1_UART_Init(void)
{
	huart1.Instance = USART1;
	huart1.Init.BaudRate = 9600;
	huart1.Init.WordLength = UART_WORDLENGTH_8B;
	huart1.Init.StopBits = UART_STOPBITS_1;
	huart1.Init.Parity = UART_PARITY_NONE;
	huart1.Init.Mode = UART_MODE_TX_RX;
	huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
	huart1.Init.OverSampling = UART_OVERSAMPLING_16;
	if (HAL_UART_Init(&huart1) != HAL_OK)
	{
		ASSERT(false);
	}
}

 

 

and

 

 

	if (uartHandle->Instance == USART1)
	{
		/* USER CODE BEGIN USART1_MspInit 0 */

		/* USER CODE END USART1_MspInit 0 */
		/* USART1 clock enable */
		__HAL_RCC_USART1_CLK_ENABLE();

		__HAL_RCC_GPIOB_CLK_ENABLE();
		__HAL_RCC_GPIOC_CLK_ENABLE();
		/**USART1 GPIO Configuration
		PC2     ------> USART1_RTS
		PC0     ------> USART1_TX
		PB0     ------> USART1_RX
		*/
		GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_2;
		GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
		GPIO_InitStruct.Pull = GPIO_NOPULL;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
		HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

		GPIO_InitStruct.Pin = GPIO_PIN_0;
		GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
		GPIO_InitStruct.Pull = GPIO_NOPULL;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
		GPIO_InitStruct.Alternate = GPIO_AF4_USART1;
		HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

		/* USART3 interrupt Init */
		GIC_SetPriority(USART1_IRQn, 0);
		GIC_EnableIRQ(USART1_IRQn);
		/* USER CODE BEGIN USART1_MspInit 1 */

		/* USER CODE END USART1_MspInit 1 */
	}

 

 

I'm wondering if this code is correct cause, connecting to the CN8 pins a 232-USB FTDI232 converter I see nothing on the terminal running on Windows.

If I comment out the GIC_EnableIRQ() lines the firmware continue to run (without any serial output): I see the firmware is alive cause a task that blinks red and blue LEDS.

If I leave the IRQ (and I transmit something) the LEDs task freeze and if I press pause IDE button I almost always land in the IRQ_EndOfInterrupt() function (or nearby - irqarmv7a.S), with irqn=70 (USART1_IRQn).

If I try with UART8 I  have the same behaviors but irqn=116 (UART8_IRQn).

Any idea, please?

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

It is a bare metal programming.

I've found the working UART1 configurations:

 

		GPIO_InitStruct.Pin = GPIO_PIN_0;
		GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
		GPIO_InitStruct.Pull = GPIO_NOPULL;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
		GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
		HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

		GPIO_InitStruct.Pin = GPIO_PIN_0;
		GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
		GPIO_InitStruct.Pull = GPIO_PULLUP;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
		GPIO_InitStruct.Alternate = GPIO_AF4_USART1;
		HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 

In general, whare I can find the possible pins configuration, including the alternate modes?

Thanks!

View solution in original post

5 REPLIES 5
SteMMo
Senior

Partial solutions:

UART8:

  • removed the __HAL_RCC_GPIOx_ENABLE() macros
  • added the UART8_IRQHandler() to overwrite the empty default function

This way I'm able to receive on Windows side the output. But on the CN8 connector there is not the UART8_RX pin.

UART1: applied the same changes. The UART1_IRQHandler() only receives FRAME_ERROR irq.

 

Following the UART8 way, I wrote some functions to handle the debug outputs toward UART8.

The source is:

 

/*
 * serial_dbg.c
 *
 *  Created on: Sep 4, 2024
 *
 */

#include <stdio.h>
#include <stdarg.h>
#include "system.h"
#include "stm32mp13xx_it.h"
#include "serial_dbg.h"


#define DBGMSG_MAX_STRING_LENGTH		128


static UART_HandleTypeDef huartDbg;
static __IO ITStatus UartReady = RESET;



void serial_dbg_output(const char *format, ...)
{
	static va_list  args;
	static uint32_t length;

	if (huartDbg.Instance == 0)	
		return;

	char Trace_Buffer[DBGMSG_MAX_STRING_LENGTH + 1];

	va_start(args, format); //lint !e718 !e727 !e746 !e530
	length = vsnprintf(Trace_Buffer, sizeof(Trace_Buffer), format, args);
	if (length > DBGMSG_MAX_STRING_LENGTH)
	{
		length = DBGMSG_MAX_STRING_LENGTH;
		Trace_Buffer[DBGMSG_MAX_STRING_LENGTH - 2] = '.';
		Trace_Buffer[DBGMSG_MAX_STRING_LENGTH - 1] = '.';
		Trace_Buffer[DBGMSG_MAX_STRING_LENGTH]     = '\0';
	}
	va_end(args); //lint !e718 !e746

	if(HAL_UART_Transmit_IT(&huartDbg, (uint8_t*)Trace_Buffer, length)!= HAL_OK)
	{
	  Error_Handler();
	}

	while (UartReady != SET){}

	/* Reset transmission flag */
	UartReady = RESET;
}


/* UARTDbg init function */
static void MX_UARTDbg_Init(void)
{
	huartDbg.Instance = UART8;
	huartDbg.Init.BaudRate = 9600;
	huartDbg.Init.WordLength = UART_WORDLENGTH_8B;
	huartDbg.Init.StopBits = UART_STOPBITS_1;
	huartDbg.Init.Parity = UART_PARITY_NONE;
	huartDbg.Init.Mode = UART_MODE_TX_RX;
  huartDbg.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huartDbg.Init.OverSampling = UART_OVERSAMPLING_16;
  huartDbg.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huartDbg.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huartDbg.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huartDbg) != HAL_OK)
  {
    Error_Handler();
  }

  if (HAL_UARTEx_SetTxFifoThreshold(&huartDbg, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }

  if (HAL_UARTEx_SetRxFifoThreshold(&huartDbg, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }

  if (HAL_UARTEx_DisableFifoMode(&huartDbg) != HAL_OK)
  {
    Error_Handler();
  }

}


/*
 */
void serial_dbg_init()
{
	char initMsg[] = "-- DEBUG STARTED --\r\n";

	MX_UARTDbg_Init();
	serial_dbg_output(initMsg);
}



void UART8_IRQHandler(void)
{
  HAL_UART_IRQHandler(&huartDbg);
}


void HAL_UART_TxCpltCallback(UART_HandleTypeDef *UartHandle)
{
  /* Set transmission flag: transfer complete */
  UartReady = SET;
}

 

The functions are callled within application_init() function, generating some debug outputs between some init functions.

Now it happens that, after the call to serial_dbg_init(), if I call a function that contains a task creation, for example

 

	Usb_App_Thread_Id = osThreadNew(usb_app_task, NULL, &Usb_App_Thread_Attributes);

 

the firmware hangs.

WhenI press pause button, I land in an infinite loop (while(1);) inside the CUndefHandler() function in the file RTX/Src/handlers.c, calld by Undef_Handler() in RTX/Src/irq_armv7a.S

Without the serial_dbg_init() call there are not problems.

Any idea?

debugging
Lead

Is this bare metal programming and the STM32MP13 or using Linux ?

It is a bare metal programming.

I've found the working UART1 configurations:

 

		GPIO_InitStruct.Pin = GPIO_PIN_0;
		GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
		GPIO_InitStruct.Pull = GPIO_NOPULL;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
		GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
		HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

		GPIO_InitStruct.Pin = GPIO_PIN_0;
		GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
		GPIO_InitStruct.Pull = GPIO_PULLUP;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
		GPIO_InitStruct.Alternate = GPIO_AF4_USART1;
		HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 

In general, whare I can find the possible pins configuration, including the alternate modes?

Thanks!

Hi @SteMMo ,

 


@SteMMo wrote:

In general, whare I can find the possible pins configuration, including the alternate modes?


 

Information is present in product Datasheet or in a more friendly way using STM32CubeMx.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here